Skip to main content
Amir1
Associate III
March 10, 2019
Question

Difficulty in Setting Interrupts

  • March 10, 2019
  • 2 replies
  • 676 views

Hello All

Could someone kindly help me figure out what may be wrong with this code (only the relevant part has been pasted here)?

The objective is to toggle the LED through interrupts coming from TIM7, the simplest timer I could setup. In despair, I have placed all the callback functions that I could find in the header file. The code compiles error free, and the initializations seem to take place with no issue. It just does not toggle the LED once it reaches the while(1) loop.

Thanks in advance

Amir

...

 ​__enable_irq();

HAL_NVIC_EnableIRQ(TIM7_IRQn);

HAL_TIM_Base_Start_IT(&htim7);

HAL_TIM_IRQHandler(&htim7);

HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET); // for test in stepped debugging mode

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin); // for test in stepped debugging mode

while (1)

{

}

}

void __HAL_TIM_OC_DelayElapsedCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void __HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void __HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void __HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void HAL_TIM_TriggerCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void HAL_TIM_ErrorCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void HAL_TIMEx_CommutationCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

void HAL_TIMEx_BreakCallback(TIM_HandleTypeDef *htim)

{

HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);

}

...

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
March 11, 2019

For IRQs to actually work you'd need an TIM7_IRQHandler() that calls HAL_TIM_IRQHandler(&htim7); when they occur, and it in turn will call your callbacks.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amir1
Amir1Author
Associate III
March 11, 2019

​Thanks. It works now.

Do you happen to have a document that explains these subtleties?

Amir