Skip to main content
Associate
Mar 27, 2025 5:46 AM UTC
Solved

DHCP error in LwIP Ethernet middleware on STM32H755 CM4

The problem ethernet link with NUCLEO-H755ZI-Q.
The conditions are as follows:

  • Board: NUCLEO-H755ZI-Q
  • Ethenet select core: CM4
  • STM32Cube_FW_H7: V1.12.1
  • LWIP: V2.1.2
  • DHCP client

In this case, the Ack from the DHCP server could not be confirmed as being received.
dhcp->pcb_allocated is set to 0 (in function of dhcp_recv()).
A similar error has not occurred with CM7.

Do you happen to know the reason for this?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 28, 2025 7:47 AM UTC

@MasatoKawatsuma wrote:

The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used

 

 No the problem in that thread is not only about the MPU configuration but also linked to the memory partition.

So check also your SRAM memory partitioning.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

5 replies

mƎALLEm
ST Technical Moderator
Mar 27, 2025 7:30 AM UTC

Hello @MasatoKawatsuma and welcome to the community,

Related question raised on this thread.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
Mar 28, 2025 7:28 AM UTC

The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used

 

Also, the following warning occurred while debugging dhcp, so I think it might be a problem with pbuf memory management.

Assertion "pbuf_free: p->ref > 0" failed at line 753 in {path}/Middlewares/Third_Party/LwIP/src/core/pbuf.c

If you know anything, please let me know.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 28, 2025 7:47 AM UTC

@MasatoKawatsuma wrote:

The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used

 

 No the problem in that thread is not only about the MPU configuration but also linked to the memory partition.

So check also your SRAM memory partitioning.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Billy OWEN
ST Employee
Mar 27, 2025 4:25 PM UTC

Hi @MasatoKawatsuma 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy