Skip to main content
timistof
Associate III
Aug 1, 2019 9:48 PM UTC
Solved

DFU bootloader for STM32F429 using external PHY?

I'm developing an STM32F429-based high-speed USB audio device that uses a Microchip USB3320 external PHY and would benefit from a DFU mode.

Is there an example available anywhere for such a configuration?

The default bootloader present in system memory doesn't seem to support the external PHY, so a bootloader that does this would reside in flash memory, similar like this project here:

https://github.com/akospasztor/stm32-bootloader

This topic has been closed for replies.
timistof
timistofBest answer
Associate III
Aug 1, 2019 10:07 PM UTC

Ah, that was obvious: there seems to be a option in CubeMX to create a DFU project. I will check that out, hope it will work with the HS PHY.

1 reply

timistof
timistofAuthorBest answer
Associate III
Aug 1, 2019 10:07 PM UTC

Ah, that was obvious: there seems to be a option in CubeMX to create a DFU project. I will check that out, hope it will work with the HS PHY.