Skip to main content
Associate
April 1, 2026
Solved

DFSDM CubeMX DMA Callback Issue

Hi 

I configured the DFSDM1 on the STM32H753VIT6 for a MEMS Mic.
I got the problem that the DMA Callback on (Half)/Full buffer never gets called. 

I used AN5027 as guideline and the DFSDM Audio Example
D-Cache disabled and set the Audio Sampling Frequency low (4kHz) to debug over UART. 

Main (snippets):

DFSDM_Filter_HandleTypeDef hdfsdm1_filter0;
DFSDM_Channel_HandleTypeDef hdfsdm1_channel4;
DMA_HandleTypeDef hdma_dfsdm1_flt0;
.
.
.
.

int32_t LeftRecBuff[1024];
void HAL_DFSDM_FilterRegConvHalfCpltCallback(DFSDM_Filter_HandleTypeDef *hdfsdm_filter)
{
/*Never Reached*/
}
int main(void)
{
 HAL_Init();
 SystemClock_Config();

/* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_DFSDM1_Init();
 /* USER CODE BEGIN 2 */

 // imu_init(&hspi4, GPIOE, GPIO_PIN_4 /* IIM-42652 CS */);
 HAL_DFSDM_FilterRegularStart_DMA(&hdfsdm1_filter0, LeftRecBuff, 1024);
while (1)
 {}
}


Config (CubeMX)

/**
 * @brief DFSDM1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DFSDM1_Init(void)
{

 /* USER CODE BEGIN DFSDM1_Init 0 */

 /* USER CODE END DFSDM1_Init 0 */

 /* USER CODE BEGIN DFSDM1_Init 1 */

 /* USER CODE END DFSDM1_Init 1 */
 hdfsdm1_filter0.Instance = DFSDM1_Filter0;
 hdfsdm1_filter0.Init.RegularParam.Trigger = DFSDM_FILTER_SW_TRIGGER;
 hdfsdm1_filter0.Init.RegularParam.FastMode = ENABLE;
 hdfsdm1_filter0.Init.RegularParam.DmaMode = ENABLE;
 hdfsdm1_filter0.Init.FilterParam.SincOrder = DFSDM_FILTER_FASTSINC_ORDER;
 hdfsdm1_filter0.Init.FilterParam.Oversampling = 750;
 hdfsdm1_filter0.Init.FilterParam.IntOversampling = 1;
 if (HAL_DFSDM_FilterInit(&hdfsdm1_filter0) != HAL_OK)
 {
 Error_Handler();
 }

 hdfsdm1_channel4.Instance = DFSDM1_Channel4;
 hdfsdm1_channel4.Init.OutputClock.Activation = ENABLE;
 hdfsdm1_channel4.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_SYSTEM;
 hdfsdm1_channel4.Init.OutputClock.Divider = 40;
 hdfsdm1_channel4.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
 hdfsdm1_channel4.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE;
 hdfsdm1_channel4.Init.Input.Pins = DFSDM_CHANNEL_SAME_CHANNEL_PINS;
 hdfsdm1_channel4.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
 hdfsdm1_channel4.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
 hdfsdm1_channel4.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER;
 hdfsdm1_channel4.Init.Awd.Oversampling = 1;
 hdfsdm1_channel4.Init.Offset = 0;
 hdfsdm1_channel4.Init.RightBitShift = 0x03;
 if (HAL_DFSDM_ChannelInit(&hdfsdm1_channel4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_DFSDM_FilterConfigRegChannel(&hdfsdm1_filter0, DFSDM_CHANNEL_4, DFSDM_CONTINUOUS_CONV_ON) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DFSDM1_Init 2 */

 /* USER CODE END DFSDM1_Init 2 */

}

 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

}

 

Khaled_DHIFBest answer
ST Employee
April 10, 2026

Hello @fwald ,

The problem is most likely the RAM location of your buffer.

On STM32H7 devices, the DMA cannot access DTCM/ITCM memories. Those memories are tightly coupled to the CPU, so even if the DFSDM is working and FLTRDATAR is changing, the DMA transfer will not complete if the destination buffer is placed there.

This is visible in the block interconnect matrix from RM0433:

Khaled_DHIF_0-1775816585229.png

 

So please make sure your buffer is located in a DMA-accessible RAM region, for example SRAM1 or SRAM2.

You can do that by placing the buffer in the proper section with an attribute macro, depending on your linker script, for example:

 
__attribute__((section(".RAM_D2")))
int32_t LeftRecBuff[1024];

or another SRAM section that is accessible by DMA in your project. 

You can find more details about this kind of issue in the community article linked here.

Also, if D-Cache is enabled later, remember that cache maintenance may be needed for DMA buffers.

So, in short:

  • DFSDM looks OK
  • DMA request / callbacks are not the real issue 
  • the buffer is probably in a memory region not reachable by DMA

Move the buffer to SRAM1/SRAM2, and the callbacks should start working. 

Best regards,

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"

15 replies

ST Technical Moderator
April 2, 2026

Hello @fwald 

Could you please share the DMA config please?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
fwaldAuthor
Associate
April 2, 2026

Hi @Saket_Om 

The DFSDM1 DMA Settings in CubeMX:

DMA Request: DFSDM1_FLT0
Stream: DMA1 Stream 0
Direction: Perpheral To Memory
Priority: High

I didnt changed anything in MDMA or BDMA. 

Th full project is also attached. 

stm32h7xx_it.c

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file stm32h7xx_it.c
 * @brief Interrupt Service Routines.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32h7xx_it.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */

/* USER CODE END TD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/* External variables --------------------------------------------------------*/
extern DMA_HandleTypeDef hdma_dfsdm1_flt0;
extern DFSDM_Filter_HandleTypeDef hdfsdm1_filter0;
/* USER CODE BEGIN EV */

/* USER CODE END EV */

/******************************************************************************/
/* Cortex Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
 * @brief This function handles Non maskable interrupt.
 */
void NMI_Handler(void)
{
 /* USER CODE BEGIN NonMaskableInt_IRQn 0 */

 /* USER CODE END NonMaskableInt_IRQn 0 */
 /* USER CODE BEGIN NonMaskableInt_IRQn 1 */
 while (1)
 {
 }
 /* USER CODE END NonMaskableInt_IRQn 1 */
}

/**
 * @brief This function handles Hard fault interrupt.
 */
void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

/**
 * @brief This function handles Memory management fault.
 */
void MemManage_Handler(void)
{
 /* USER CODE BEGIN MemoryManagement_IRQn 0 */

 /* USER CODE END MemoryManagement_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_MemoryManagement_IRQn 0 */
 /* USER CODE END W1_MemoryManagement_IRQn 0 */
 }
}

/**
 * @brief This function handles Pre-fetch fault, memory access fault.
 */
void BusFault_Handler(void)
{
 /* USER CODE BEGIN BusFault_IRQn 0 */

 /* USER CODE END BusFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_BusFault_IRQn 0 */
 /* USER CODE END W1_BusFault_IRQn 0 */
 }
}

/**
 * @brief This function handles Undefined instruction or illegal state.
 */
void UsageFault_Handler(void)
{
 /* USER CODE BEGIN UsageFault_IRQn 0 */

 /* USER CODE END UsageFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_UsageFault_IRQn 0 */
 /* USER CODE END W1_UsageFault_IRQn 0 */
 }
}

/**
 * @brief This function handles System service call via SWI instruction.
 */
void SVC_Handler(void)
{
 /* USER CODE BEGIN SVCall_IRQn 0 */

 /* USER CODE END SVCall_IRQn 0 */
 /* USER CODE BEGIN SVCall_IRQn 1 */

 /* USER CODE END SVCall_IRQn 1 */
}

/**
 * @brief This function handles Debug monitor.
 */
void DebugMon_Handler(void)
{
 /* USER CODE BEGIN DebugMonitor_IRQn 0 */

 /* USER CODE END DebugMonitor_IRQn 0 */
 /* USER CODE BEGIN DebugMonitor_IRQn 1 */

 /* USER CODE END DebugMonitor_IRQn 1 */
}

/**
 * @brief This function handles Pendable request for system service.
 */
void PendSV_Handler(void)
{
 /* USER CODE BEGIN PendSV_IRQn 0 */

 /* USER CODE END PendSV_IRQn 0 */
 /* USER CODE BEGIN PendSV_IRQn 1 */

 /* USER CODE END PendSV_IRQn 1 */
}

/**
 * @brief This function handles System tick timer.
 */
void SysTick_Handler(void)
{
 /* USER CODE BEGIN SysTick_IRQn 0 */

 /* USER CODE END SysTick_IRQn 0 */
 HAL_IncTick();
 /* USER CODE BEGIN SysTick_IRQn 1 */

 /* USER CODE END SysTick_IRQn 1 */
}

/******************************************************************************/
/* STM32H7xx Peripheral Interrupt Handlers */
/* Add here the Interrupt Handlers for the used peripherals. */
/* For the available peripheral interrupt handler names, */
/* please refer to the startup file (startup_stm32h7xx.s). */
/******************************************************************************/

/**
 * @brief This function handles DMA1 stream0 global interrupt.
 */
void DMA1_Stream0_IRQHandler(void)
{
 /* USER CODE BEGIN DMA1_Stream0_IRQn 0 */

 /* USER CODE END DMA1_Stream0_IRQn 0 */
 HAL_DMA_IRQHandler(&hdma_dfsdm1_flt0);
 /* USER CODE BEGIN DMA1_Stream0_IRQn 1 */

 /* USER CODE END DMA1_Stream0_IRQn 1 */
}

/**
 * @brief This function handles DFSDM1 filter0 global interrupt.
 */
void DFSDM1_FLT0_IRQHandler(void)
{
 /* USER CODE BEGIN DFSDM1_FLT0_IRQn 0 */

 /* USER CODE END DFSDM1_FLT0_IRQn 0 */
 HAL_DFSDM_IRQHandler(&hdfsdm1_filter0);
 /* USER CODE BEGIN DFSDM1_FLT0_IRQn 1 */

 /* USER CODE END DFSDM1_FLT0_IRQn 1 */
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

stm32h7xx_hal_msp.c

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file stm32h7xx_hal_msp.c
 * @brief This file provides code for the MSP Initialization
 * and de-Initialization codes.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */
extern DMA_HandleTypeDef hdma_dfsdm1_flt0;

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */

/* USER CODE END TD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN Define */

/* USER CODE END Define */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN Macro */

/* USER CODE END Macro */

/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* External functions --------------------------------------------------------*/
/* USER CODE BEGIN ExternalFunctions */

/* USER CODE END ExternalFunctions */

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */
/**
 * Initializes the Global MSP.
 */
void HAL_MspInit(void)
{

 /* USER CODE BEGIN MspInit 0 */

 /* USER CODE END MspInit 0 */

 __HAL_RCC_SYSCFG_CLK_ENABLE();

 /* System interrupt init*/

 /* USER CODE BEGIN MspInit 1 */

 /* USER CODE END MspInit 1 */
}

static uint32_t HAL_RCC_DFSDM1_CLK_ENABLED=0;

static uint32_t DFSDM1_Init = 0;
/**
 * @brief DFSDM_Filter MSP Initialization
 * This function configures the hardware resources used in this example
 * hdfsdm_filter: DFSDM_Filter handle pointer
 * @retval None
 */
void HAL_DFSDM_FilterMspInit(DFSDM_Filter_HandleTypeDef* hdfsdm_filter)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspInit 0 */

 /* USER CODE END DFSDM1_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DFSDM1;
 PeriphClkInitStruct.Dfsdm1ClockSelection = RCC_DFSDM1CLKSOURCE_D2PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 HAL_RCC_DFSDM1_CLK_ENABLED++;
 if(HAL_RCC_DFSDM1_CLK_ENABLED==1){
 __HAL_RCC_DFSDM1_CLK_ENABLE();
 }

 __HAL_RCC_GPIOE_CLK_ENABLE();
 /**DFSDM1 GPIO Configuration
 PE9 ------> DFSDM1_CKOUT
 PE10 ------> DFSDM1_DATIN4
 */
 GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF3_DFSDM1;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /* DFSDM1 interrupt Init */
 HAL_NVIC_SetPriority(DFSDM1_FLT0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DFSDM1_FLT0_IRQn);
 /* USER CODE BEGIN DFSDM1_MspInit 1 */

 /* USER CODE END DFSDM1_MspInit 1 */

 DFSDM1_Init++;
 }

 /* DFSDM1 DMA Init */
 /* DFSDM1_FLT0 Init */
 if(hdfsdm_filter->Instance == DFSDM1_Filter0){
 hdma_dfsdm1_flt0.Instance = DMA1_Stream0;
 hdma_dfsdm1_flt0.Init.Request = DMA_REQUEST_DFSDM1_FLT0;
 hdma_dfsdm1_flt0.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_dfsdm1_flt0.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_dfsdm1_flt0.Init.MemInc = DMA_MINC_ENABLE;
 hdma_dfsdm1_flt0.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_dfsdm1_flt0.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_dfsdm1_flt0.Init.Mode = DMA_CIRCULAR;
 hdma_dfsdm1_flt0.Init.Priority = DMA_PRIORITY_HIGH;
 hdma_dfsdm1_flt0.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_dfsdm1_flt0) != HAL_OK)
 {
 Error_Handler();
 }

 /* Several peripheral DMA handle pointers point to the same DMA handle.
 Be aware that there is only one channel to perform all the requested DMAs. */
 __HAL_LINKDMA(hdfsdm_filter,hdmaInj,hdma_dfsdm1_flt0);
 __HAL_LINKDMA(hdfsdm_filter,hdmaReg,hdma_dfsdm1_flt0);
 }

}

/**
 * @brief DFSDM_Channel MSP Initialization
 * This function configures the hardware resources used in this example
 * hdfsdm_channel: DFSDM_Channel handle pointer
 * @retval None
 */
void HAL_DFSDM_ChannelMspInit(DFSDM_Channel_HandleTypeDef* hdfsdm_channel)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspInit 0 */

 /* USER CODE END DFSDM1_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DFSDM1;
 PeriphClkInitStruct.Dfsdm1ClockSelection = RCC_DFSDM1CLKSOURCE_D2PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 HAL_RCC_DFSDM1_CLK_ENABLED++;
 if(HAL_RCC_DFSDM1_CLK_ENABLED==1){
 __HAL_RCC_DFSDM1_CLK_ENABLE();
 }

 __HAL_RCC_GPIOE_CLK_ENABLE();
 /**DFSDM1 GPIO Configuration
 PE9 ------> DFSDM1_CKOUT
 PE10 ------> DFSDM1_DATIN4
 */
 GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF3_DFSDM1;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /* USER CODE BEGIN DFSDM1_MspInit 1 */

 /* USER CODE END DFSDM1_MspInit 1 */

 DFSDM1_Init++;
 }

}

/**
 * @brief DFSDM_Filter MSP De-Initialization
 * This function freeze the hardware resources used in this example
 * hdfsdm_filter: DFSDM_Filter handle pointer
 * @retval None
 */
void HAL_DFSDM_FilterMspDeInit(DFSDM_Filter_HandleTypeDef* hdfsdm_filter)
{
 DFSDM1_Init-- ;
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspDeInit 0 */

 /* USER CODE END DFSDM1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_DFSDM1_CLK_DISABLE();

 /**DFSDM1 GPIO Configuration
 PE9 ------> DFSDM1_CKOUT
 PE10 ------> DFSDM1_DATIN4
 */
 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_9|GPIO_PIN_10);

 /* DFSDM1 interrupt DeInit */
 HAL_NVIC_DisableIRQ(DFSDM1_FLT0_IRQn);

 /* DFSDM1 DMA DeInit */
 HAL_DMA_DeInit(hdfsdm_filter->hdmaInj);
 HAL_DMA_DeInit(hdfsdm_filter->hdmaReg);
 /* USER CODE BEGIN DFSDM1_MspDeInit 1 */

 /* USER CODE END DFSDM1_MspDeInit 1 */
 }

}

/**
 * @brief DFSDM_Channel MSP De-Initialization
 * This function freeze the hardware resources used in this example
 * hdfsdm_channel: DFSDM_Channel handle pointer
 * @retval None
 */
void HAL_DFSDM_ChannelMspDeInit(DFSDM_Channel_HandleTypeDef* hdfsdm_channel)
{
 DFSDM1_Init-- ;
 if(DFSDM1_Init == 0)
 {
 /* USER CODE BEGIN DFSDM1_MspDeInit 0 */

 /* USER CODE END DFSDM1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_DFSDM1_CLK_DISABLE();

 /**DFSDM1 GPIO Configuration
 PE9 ------> DFSDM1_CKOUT
 PE10 ------> DFSDM1_DATIN4
 */
 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_9|GPIO_PIN_10);

 /* USER CODE BEGIN DFSDM1_MspDeInit 1 */

 /* USER CODE END DFSDM1_MspDeInit 1 */
 }

}

/**
 * @brief UART MSP Initialization
 * This function configures the hardware resources used in this example
 * huart: UART handle pointer
 * @retval None
 */
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(huart->Instance==UART4)
 {
 /* USER CODE BEGIN UART4_MspInit 0 */

 /* USER CODE END UART4_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_UART4;
 PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Peripheral clock enable */
 __HAL_RCC_UART4_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**UART4 GPIO Configuration
 PA11 ------> UART4_RX
 PA12 ------> UART4_TX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_UART4;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* USER CODE BEGIN UART4_MspInit 1 */

 /* USER CODE END UART4_MspInit 1 */

 }

}

/**
 * @brief UART MSP De-Initialization
 * This function freeze the hardware resources used in this example
 * huart: UART handle pointer
 * @retval None
 */
void HAL_UART_MspDeInit(UART_HandleTypeDef* huart)
{
 if(huart->Instance==UART4)
 {
 /* USER CODE BEGIN UART4_MspDeInit 0 */

 /* USER CODE END UART4_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_UART4_CLK_DISABLE();

 /**UART4 GPIO Configuration
 PA11 ------> UART4_RX
 PA12 ------> UART4_TX
 */
 HAL_GPIO_DeInit(GPIOA, GPIO_PIN_11|GPIO_PIN_12);

 /* USER CODE BEGIN UART4_MspDeInit 1 */

 /* USER CODE END UART4_MspDeInit 1 */
 }

}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

 

main.c

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "stm32h7xx_hal.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

DFSDM_Filter_HandleTypeDef hdfsdm1_filter0;
DFSDM_Channel_HandleTypeDef hdfsdm1_channel4;
DMA_HandleTypeDef hdma_dfsdm1_flt0;

UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_DFSDM1_Init(void);
static void MX_UART4_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
int32_t LeftRecBuff[512];
volatile int half = 0;
void HAL_DFSDM_FilterRegConvHalfCpltCallback(DFSDM_Filter_HandleTypeDef *hdfsdm_filter)
{
 half = 1;
}
int _write(int file, char *ptr, int len)
{
 HAL_UART_Transmit(&huart4, (uint8_t *)ptr, len, HAL_MAX_DELAY);
 return len;
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_DFSDM1_Init();
 MX_UART4_Init();
 /* USER CODE BEGIN 2 */
 printf("Start DFSDM1\n");
 HAL_DFSDM_FilterRegularStart_DMA(&hdfsdm1_filter0, LeftRecBuff, sizeof(LeftRecBuff));
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 printf("First Element: %ld\n", LeftRecBuff[0]);
 HAL_Delay(100);
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 5;
 RCC_OscInitStruct.PLL.PLLN = 192;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief DFSDM1 Initialization Function
 * None
 * @retval None
 */
static void MX_DFSDM1_Init(void)
{

 /* USER CODE BEGIN DFSDM1_Init 0 */

 /* USER CODE END DFSDM1_Init 0 */

 /* USER CODE BEGIN DFSDM1_Init 1 */

 /* USER CODE END DFSDM1_Init 1 */
 hdfsdm1_filter0.Instance = DFSDM1_Filter0;
 hdfsdm1_filter0.Init.RegularParam.Trigger = DFSDM_FILTER_SW_TRIGGER;
 hdfsdm1_filter0.Init.RegularParam.FastMode = ENABLE;
 hdfsdm1_filter0.Init.RegularParam.DmaMode = ENABLE;
 hdfsdm1_filter0.Init.FilterParam.SincOrder = DFSDM_FILTER_FASTSINC_ORDER;
 hdfsdm1_filter0.Init.FilterParam.Oversampling = 750;
 hdfsdm1_filter0.Init.FilterParam.IntOversampling = 1;
 if (HAL_DFSDM_FilterInit(&hdfsdm1_filter0) != HAL_OK)
 {
 Error_Handler();
 }
 hdfsdm1_channel4.Instance = DFSDM1_Channel4;
 hdfsdm1_channel4.Init.OutputClock.Activation = ENABLE;
 hdfsdm1_channel4.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_SYSTEM;
 hdfsdm1_channel4.Init.OutputClock.Divider = 40;
 hdfsdm1_channel4.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
 hdfsdm1_channel4.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE;
 hdfsdm1_channel4.Init.Input.Pins = DFSDM_CHANNEL_SAME_CHANNEL_PINS;
 hdfsdm1_channel4.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
 hdfsdm1_channel4.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
 hdfsdm1_channel4.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER;
 hdfsdm1_channel4.Init.Awd.Oversampling = 1;
 hdfsdm1_channel4.Init.Offset = 0;
 hdfsdm1_channel4.Init.RightBitShift = 2;
 if (HAL_DFSDM_ChannelInit(&hdfsdm1_channel4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_DFSDM_FilterConfigRegChannel(&hdfsdm1_filter0, DFSDM_CHANNEL_4, DFSDM_CONTINUOUS_CONV_ON) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DFSDM1_Init 2 */

 /* USER CODE END DFSDM1_Init 2 */

}

/**
 * @brief UART4 Initialization Function
 * None
 * @retval None
 */
static void MX_UART4_Init(void)
{

 /* USER CODE BEGIN UART4_Init 0 */

 /* USER CODE END UART4_Init 0 */

 /* USER CODE BEGIN UART4_Init 1 */

 /* USER CODE END UART4_Init 1 */
 huart4.Instance = UART4;
 huart4.Init.BaudRate = 115200;
 huart4.Init.WordLength = UART_WORDLENGTH_8B;
 huart4.Init.StopBits = UART_STOPBITS_1;
 huart4.Init.Parity = UART_PARITY_NONE;
 huart4.Init.Mode = UART_MODE_TX_RX;
 huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart4.Init.OverSampling = UART_OVERSAMPLING_16;
 huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART4_Init 2 */

 /* USER CODE END UART4_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

ST Technical Moderator
April 2, 2026

Hello @fwald 

HAL_DFSDM_FilterRegularStart_DMA() expects the number of 32‑bit samples, not the number of bytes. With sizeof(LeftRecBuff) you are passing 512 * 4 = 2048, so the DMA is configured to transfer 2048 words, but your buffer has space for only 512 words

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
fwaldAuthor
Associate
April 7, 2026

hi @Saket_Om 

I divided the length variable by 4 but it didn't triggered the Callback. I doubled checked the Examples Main File there the length is also given in bytes and the DMA's Data Width is set to Word.
Changing the Data Width as Byte in the DFSDM1 DMA Settings didn't solved the problem either. 

April 2, 2026

Looks like your DMA callbacks aren’t triggering. Double-check that:

  1. DFSDM trigger is correctly set (SW_TRIGGER may need manual start).
  2. DMA IRQ vector matches the stream used.
  3. Cache/Memory issues: you disabled D-Cache, good, but also ensure LeftRecBuff is aligned.

Sometimes using DFSDM_FILTER_SYNC_TRIGGER instead of SW_TRIGGER solves callback issues. Also, make sure HAL_DFSDM_FilterRegularStart_DMA() is actually returning HAL_OK.

fwaldAuthor
Associate
April 7, 2026

Hi @unknown 

Thanks for the inputs. 

- SW_Trigger Manual start didn't change behaviour. The register was already correct. 

- Stream and IRQ Vector matches

- I applied now the ALIGN_32BYTES(...); no difference.

- Setting DFSDM_FILTER_SYNC_TRIGGER results an error in HAL_DFSDM_FilterInit.

- HAL_DFSDM_FilterRegularStart_DMA() returns HAL_OK. 

 

fwaldAuthor
Associate
April 7, 2026

FYI @Saket_Om @unknown 

Using the DFSDM without DMA or IT, just simply polling, seems to work. I can read out data and send a downsampled signal over UART, that somehow sounds like a very bad recording. 
But polling isn't an option. 

ST Technical Moderator
April 7, 2026

Great news!

In this case try to use the same DMA setting as in the example and check the result.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
fwaldAuthor
Associate
April 7, 2026

Added the DMA with the same settings, double checked. Same outcome. 

Difference I found:
- The HAL_DMA_IRQHandler in the examples takes the hdmaReg but that seems not possible in stm32h7xx_it.c only a pointer of the dfsdm_handler. (Guess its ok)
- DMA_Init() is after the DFSDM_Init() in the example. Changed it in my code but no difference. 

Added the current project. 

fwaldAuthor
Associate
April 9, 2026

Can someone help me here out?

If checked the register values and it seems all fine to me. But the DMA dont grab the data
after HAL_DFSDM_FilterRegularStart_DMA()

DFSDM1_Filter0
- FLTCR1 = 606339073
- FLTISR = 16728074
- FLTRDATAR = is changing
The DFSDM is therefore reading the Mic data

DMAMUX1_Channel1
- CCR = 101   (dfsdm1_dma0)

The DMA Handler hdma_dfsdm1_flt0
- Init->Request = 101 (so matches the MUX CCR)

DMA1_Stream1
- CR =  218394
- M0AR = 536871496 matches the address of the Buffer (0x20000248 <LeftRecBuff>)
- PAR = 1073836316 matches the addess of the &DFSDM1_Filter0.FLTRDATAR 0x4001711c

In my understanding the data gets read from the input gets filtered and placed in the Filters data register. The DMA should start and has the correct register to read from and right to. Whats wrong?





ST Technical Moderator
April 9, 2026

Hello @fwald 

Did you check the return value of HAL_DFSDM_FilterRegularStart_DMA() ?

if (HAL_DFSDM_FilterRegularStart_DMA(&hdfsdm1_filter0, LeftRecBuff, 1024) != HAL_OK)

{

  while(1);

}

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
fwaldAuthor
Associate
April 9, 2026

Yes returns HAL_OK 

fwaldAuthor
Associate
April 9, 2026

It seems a DMA Problem. I tried a simple UART_Transmit_DMA (Example: GettingStarted ) and it didnt work either. 
Without DMA no problem.
Tried another MCU same issue.


Khaled_DHIFBest answer
ST Employee
April 10, 2026

Hello @fwald ,

The problem is most likely the RAM location of your buffer.

On STM32H7 devices, the DMA cannot access DTCM/ITCM memories. Those memories are tightly coupled to the CPU, so even if the DFSDM is working and FLTRDATAR is changing, the DMA transfer will not complete if the destination buffer is placed there.

This is visible in the block interconnect matrix from RM0433:

Khaled_DHIF_0-1775816585229.png

 

So please make sure your buffer is located in a DMA-accessible RAM region, for example SRAM1 or SRAM2.

You can do that by placing the buffer in the proper section with an attribute macro, depending on your linker script, for example:

 
__attribute__((section(".RAM_D2")))
int32_t LeftRecBuff[1024];

or another SRAM section that is accessible by DMA in your project. 

You can find more details about this kind of issue in the community article linked here.

Also, if D-Cache is enabled later, remember that cache maintenance may be needed for DMA buffers.

So, in short:

  • DFSDM looks OK
  • DMA request / callbacks are not the real issue 
  • the buffer is probably in a memory region not reachable by DMA

Move the buffer to SRAM1/SRAM2, and the callbacks should start working. 

Best regards,

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"
fwaldAuthor
Associate
April 10, 2026

Hi @Khaled_DHIF  thanks you very much. I came across the article yesterday as well which solved the problem.

But I have to say, it is a bit frustrating that the default configuration in CubeMX doesn't work when using DMA.
Maybe I missed it, but in CubeMX should at least be a obvious message or warning pointing to the article. That would have saved me—and probably other users as well—a lot of bother.

Glad it works now. :)

Kind Regards
F.