Skip to main content
darla14
Associate III
August 5, 2026
Question

Definitive guide for interfacing PDM microphones with MDF/ADF

Hello,

is there a definitive application note to interface PDM mics with MDF/ADF?

there is AN5027 but it doesn’t tell about MDF or ADF. 
If I insert correctly MDF/ADF is a newer version of DFSDM but I would like if someone can point me to the interfacing wet stm32cubeMX for MDF/ADF usage with PDM mics showing  configurations to interface N number of MICs(1-8) for a required sampling rate(16-96 KHz) if possible?

which one to choose MDF or ADF?or both are same?

Thanks a lot in advance !

regards,

S 

4 replies

ST Technical Moderator
August 6, 2026

Hello ​@darla14 

Please refer to the application note AN5795

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
darla14
darla14Author
Associate III
August 9, 2026

Thanks ​@Saket_Om checking it.

regards

 

darla14
darla14Author
Associate III
August 10, 2026

I checked this but there is no STM32CubeMX configuration for the MDF and except the good theory portion.

regards,

 

ST Technical Moderator
August 11, 2026

Hello ​@darla14 

To configure the MDF peripheral with CubeMX please check the example below:

STM32CubeN6/Projects/STM32N6570-DK/Examples/MDF/MDF_AudioRecorder at main · STMicroelectronics/STM32CubeN6

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om