Skip to main content
PB S.1
Associate II
Jan 23, 2024 5:03 AM UTC
Question

Decompression of SD card Files

Hi,

I am using STM32H5 microcontroller with Free-RTOS environment.

Interfaced SD card with the MCU using LittleFS file system.

My SD card has Compressed files, I wanted to decompress them and write to the separate folder. Is there any libraries supported to carryout this procedure in Free-RTOS environment?

Provide if there is any example code

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Jan 23, 2024 9:42 AM UTC

@PB S.1 wrote:

My SD card has Compressed files, I wanted to decompress them 


Is it a standard compression scheme?

If so, just search for libraries for that scheme - that fact that the file is on an SD Card makes no difference.

GitHub is a good place to search for such things.

 


@PB S.1 wrote:

Is there any libraries supported to carryout this procedure in Free-RTOS environment?


That would be a question for Free-RTOS:

https://www.freertos.org/libraries/categories.html

https://www.freertos.org/FAQ.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PB S.1
PB S.1Author
Associate II
Jan 30, 2024 11:41 AM UTC

Hi Team,

Is there a PC-based tool available for storing files on an SD card in the LittleFS file system format? I aim to access and read these files using an STM32H5 MCU-based application, which already has the LittleFS file system implemented.

Andrew Neil
Super User
Jan 30, 2024 12:19 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Jan 30, 2024 12:30 PM UTC

Isn't one of the benefits of using standard file systems and file formats that you cN just copy files without having to install things on the host. Also why attaching as an USB MSC is also popular.

ZIP files use a couple of compression formats that can be implemented. Files typically need to be processed in a linear fashion where you have read and write functions that pace based on data consumption and generation, as it's often impractical to load the whole image into memory at once. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lead II
Jan 31, 2024 6:15 AM UTC

If you have a file system working which stores files on SD card, e.g. in a FAT/FAT32/exFAT formatted disk - you should be able to read/write the card also on a host computer (e.g. Windows).

If you want to "unzip" a compressed file on SD card - done by MCU FW:

  • potentially you find a "zip/unzip" library to do so: just try to add to your FW system
  • but bear in mind the size of temporary memory you would need:
    often, ZIP, using a "Huffman Coding" algorithm, might need to have the entire file content in memory first,
    or the unzipped file content needs a lot of memory where to store temporarily.

I agree with Tesla DeLorean: ZIP/UNZIP on embedded systems can be challenging in terms of memory space you need.

If you store the files on a SD Card and you have an USB connection: you could think about to implement a USB storage device, a MSC Class: then you can see your SD Card on a PC like an external memory device (via USB).

The PC can do the ZIP/UNZIP, without to take the SD Card to the PC: your SD Card in MCU pops up as a USB memory device on the host (it works well for me).

Andrew Neil
Super User
Jan 31, 2024 9:29 AM UTC

@tjaekel wrote:

If you have a file system working which stores files on SD card, e.g. in a FAT/FAT32/exFAT 


OP states LittleFS is used - not something that PCs support!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.