Skip to main content
Associate III
Dec 15, 2025 11:17 AM UTC
Question

data sharing between the cores

Hi,

I'm using STM32H7 dual core, where the data has to be shared between the cores, so im having totally 21 variables totally 76 bytes, thought of do it like a structure, so where to place the structure exactly for this data sharing. so, this structure should be placed in any linker file of one of the cores or where?

if so, thus we have to keep the structure in both the core or what

which method is a fastest wat to share the data, like a ring buffer, HSEM.

if we use HSEM, we can use that structure or access outside, before calling the HSEM TAKE, or structure values should be assigned only inside after the HSEM TAKEOVER.

 

 

regards,

srinath

3 replies

Andrew Neil
Super User
Dec 15, 2025 11:20 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Dec 15, 2025 11:34 AM UTC
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Dec 15, 2025 11:42 AM UTC

@Srinath_03 which also shows up in the Knowledgebase search results ...

 

PS:

More on OpenAMP (Open Asymmetric Multi-Processing):

https://www.openampproject.org/

https://github.com/OpenAMP/open-amp 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.