Skip to main content
Associate III
June 16, 2026
Question

D cache blocks whole running program on Nucleo h7s3l8 (even if MPU configured)

As the title suggests My program on a Nucleo H7S3L8 stops running when D cache is enabled (appearently it does not go into Hardfault mode). However, when the line SCB_EnableDCache() is commented, it starts again running. Since I need D cache I configured the MPU for where the dma buffers of the project are located, since I’ve read that it could be a cache coherency problem with DMAs, but neither this solution solves the problem. I’ve read somewhere that is XSPI2_HSLV OTP that must be enabled on STM32CubeProgrammer, but I’ve checked and this is enabled! How the problem can be solved? I’ll upload the project

3 replies

Pavel A.
June 17, 2026

In your .ld file the appli XSPI memory is mapped at 0x70000000.

But in your MPU_Config (main.c) there’s no definition for this address range, and the whole function is just buggy and does not do what intended. Please review it.

 

s319189Author
Associate III
June 17, 2026

I’ve created a new project without touching the standard configuration for MPU and I admit you were right, now the yello led blinking means that program is running. However, I2S peripherals still have cache coherency problem even if using SCB_InvalidateDCache and SCB_CleanDCache() instead of MPU config. I don’t what is a concrete working solution that solves even Cache coherency problem of I2S peripherals

ST Technical Moderator
June 18, 2026

Hello ​@s319189 

If you want to keep the I2S DMA buffer region cacheable for performance, you must strictly respect the cache line constraints below:

  • Each I2S DMA buffer must start at a 32‑byte aligned address.
  • Each buffer size must be a multiple of 32 bytes.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om