Skip to main content
abarrotes
Associate
Nov 25, 2016 11:33 PM UTC
Question

Custom bootloader STM32F405VG

Posted on November 26, 2016 at 00:33

Hello,

I'm working in a custom bootloader. I have follow many discussions here and then i end up with this code.

commenting the function PerformFirmwareUpdate() the code works ok!  

pFunction appEntry;

uint32_t appStack;

HAL_Init();

/* Get the application stack pointer (First entry in the application vector table) */

appStack = (uint32_t) *((__IO uint32_t*)EXEC_ZONE_ADDR);

/* Get the application entry point (Second entry in the application vector table) */

appEntry = (pFunction) *(__IO uint32_t*) (EXEC_ZONE_ADDR);// + 4);

if (CheckFirmwareUpdate)

//PerformFirmwareUpdate();

HAL_DeInit();

/* Reconfigure vector table offset register to match the application location */

SCB->VTOR = EXEC_ZONE_ADDR;

/* Set the application stack pointer */

__disable_irq();

__set_MSP(appStack);

__DSB();

/* Start the application */

appEntry();

when i uncomment the function which copies the program in the execution sector (5), then i get the problem:

the 

appEntry gets the value of sector 6 instead of sector 5 which is the real value assigned.

void PerformFirmwareUpdate(void)

{

if (FlashErase(FLASH_SECTOR_5))//(FLASH_SECTOR_5);

{

uint32_t *data_ptr = (uint32_t *)PROG_ZONE_ADDR;

HAL_FLASH_Unlock();

for(uint32_t i = 0; i < (SECTOR_SIZE); i += sizeof(uint32_t), data_ptr++ )

{

if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, EXEC_ZONE_ADDR + i, *data_ptr) != HAL_OK)

{ //WORD = 32bits

break;

}

FLASH_WaitForLastOperation (4000); //in ms, max time to erase whole sector; see datasheet

}

HAL_FLASH_Lock();

}

return;

}

Thanks to all, I hope someone could help me with this!

#stm2 #bootloader #stm32f4 #!stm32-!bootloader #c
This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
Nov 28, 2016 3:17 AM UTC
Posted on November 28, 2016 at 04:17

Ok, so why build it for 0x08040000? If you have it as a binary blob you can write it at any address you want. I wouldn't need a .HEX file

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Nov 28, 2016 3:23 AM UTC
Posted on November 28, 2016 at 04:23

Build the code for 0x08020000, I'd take that either as an .ELF/AXF or .HEX, convert that to a binary image suitable for flashing, with a CRC added on the end to ensure the integrity of the image.  The loader could check this prior to jumping to the new image, or copying from 0x08040000 to 0x08020000

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
abarrotes
abarrotesAuthor
Associate
Nov 30, 2016 1:26 AM UTC
Posted on November 30, 2016 at 02:26

abarrotes
abarrotesAuthor
Associate
Dec 2, 2016 2:03 AM UTC
Posted on December 02, 2016 at 03:03

Clive the problem was solved, thanks for your help!

1) My hextobin.exe was not converting properly! 

I'm using the keil tool fromelf.exe instead and right now things are working.

2) I'm using the STM u-link utility to load the bin directly