Skip to main content
RMart.0
Associate III
Oct 28, 2019 5:05 PM UTC
Solved

CubeMx generated code for STM32h7 when QuadSPi enabled but sd card disabled not compiling (perhaps bug in generated code)

When I generate code for the STM32h750 via cubeMX, I see in stm32h7xx_ll_delayblock.h:

#if defined(HAL_SD_MODULE_ENABLED) || defined(HAL_QSPI_MODULE_ENABLED)

I have QSPI enabled, but SD disabled, and the code following the #if is accounted for in the compilation, as expected. This code makes use of a const called DLYB_MAX_UNIT.

The issue is that stm32h7xx_ll_delayblock.h, which contains the definition for DLYB_MAX_UNIT is never included when SD is disabled.

This seems to be a bug either in the #if mentioned above (which should not contain the || defined(HAL_QSPI_MODULE_ENABLED)) or in the stm32h7xx_hal_qspi.h file, which does not include "stm32h7xx_ll_delayblock.h".

Notice that if SD card is enabled, the code should compile because of the following lines in stm32h7xx_hal_sd.h:

#if defined (DLYB_SDMMC1) || defined (DLYB_SDMMC2) || defined (DLYB_SDMMC3)

#include "stm32h7xx_ll_delayblock.h"

#endif /* (DLYB_SDMMC1) || (DLYB_SDMMC2) */

My STM32H7 package is V1.5.0

This topic has been closed for replies.
RMart.0
RMart.0Best answer
Associate III
Jan 8, 2020 12:22 PM UTC

The issue can not be reproduced after updating to cubemx 5.4 and STM32H7 package V1.6.0

3 replies

Amel NASRI
ST Technical Moderator
Nov 19, 2019 3:26 PM UTC

Hello @RMart.0​ ,

The functions defined in stm32h7xx_ll_delayblock.c are only used with SD module.

I assume that there is no need for the check "defined(HAL_QSPI_MODULE_ENABLED)".

Anyway, it will not generate a compilation error. But I will check with our development team to remove the non-needed check, unless it has a particular use-case that they will explain.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Amel NASRI
ST Technical Moderator
Nov 19, 2019 3:55 PM UTC

Reading again the summary of your question: you said that generated code is not compiling.

Could you please share the .ioc file leading to this issue?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
RMart.0
RMart.0AuthorBest answer
Associate III
Jan 8, 2020 12:22 PM UTC

The issue can not be reproduced after updating to cubemx 5.4 and STM32H7 package V1.6.0