Skip to main content
Associate II
Jul 2, 2024 6:45 AM UTC
Solved

cube MX issues with STM32U585OIY6QTR

 

 

Hello,

I'm currently using STM32CubeIDE, version 1.15.1 (Build: 21094_20240412_1041 UTC), with the embedded package version 1.5.0. I have set up a project with a secure zone configuration.

After generating code from the IOC file, I encounter an issue in the flash.c file at line 54. The generated code looks like this:

 

//!!! HAL_FLASHEx_OBProgram is commented because some parameters are missing

//pOBInit.OptionType = OPTIONBYTE_USER|OPTIONBYTE_BOOTADDR

|OPTIONBYTE_WMSEC;

//pOBInit.WMSecStartPage = 0;

//pOBInit.WMSecEndPage = 126;

//HAL_FLASHEx_OBProgram(&pOBInit);

 

//!!! HAL_FLASHEx_OBProgram is commented because some parameters are missing

//pOBInit.OptionType = OPTIONBYTE_USER|OPTIONBYTE_BOOTADDR

|OPTIONBYTE_WMSEC;

 

 

The OPTIONBYTE_WMSEC parameter is on the next line of the comment, which causes it to be ignored by the //. This obviously breaks the build.

While this is easy to fix manually, I have to go back and correct this every time I regenerate the code from the IOC file. Has anyone else experienced this issue or found a more permanent solution?

Thanks in advance!

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Dec 2, 2024 9:55 AM UTC

Hello @JulioAndrade @dhs 

This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

nouirakh
ST Employee
Jul 2, 2024 1:53 PM UTC

Hello @JulioAndrade, 

Could you please, provide more details about which MX version are you using?
Also could you please attach your .Ioc file/configuration or another Ioc that contains the same possible issue? This would help us to reproduce the issue and find a solution.

Senior
Nov 10, 2024 12:57 PM UTC

Same Issue, problem arise using Tools > Memory Management

 

Daniel H Sagarra
Associate II
Jul 3, 2024 8:48 AM UTC

Hello i am using 
STM32CubeIDE Version: 1.15.1 Build: 21094_20240412_1041 (UTC)

STTwo-32
ST Technical Moderator
Nov 10, 2024 2:24 PM UTC

Hello @JulioAndrade @dhs 

For the issue reported by @JulioAndrade I've been able to reproduce it and I've escalated for correction on the future (under internal ticket number 196056). For the project that you have attached @dhs , the .ioc file generated works fine with the last version of STM32CubeIDE (V 1.16.1). 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Senior
Nov 10, 2024 3:55 PM UTC

@STTwo-32 

In my case:

- A warring arise, this is easy to fix

- Additionally, I have to edit to add the parameter  NOLOAD every time I regenerate: 

 

/* Unitialized RAM_BACKUP section into "RAM_BACKUP" RAM_BACKUP type memory */

.RAM_BACKUP_Section(NOLOAD) :

{

. = ALIGN(4);

KEEP (*(.RAM_BACKUP_Section))

. = ALIGN(4);

} >RAM_BACKUP

Daniel H Sagarra
STTwo-32
ST Technical Moderator
Nov 10, 2024 4:11 PM UTC

This is not the same behavior of the original post. I suggest you to create a new post for it with more details (how to reproduce, the version of IDE/MX YOU are using, some screenshots,...) 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Dec 2, 2024 9:55 AM UTC

Hello @JulioAndrade @dhs 

This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.