Question
Cube F7 1.7.0 CAN library bug?
Posted on May 02, 2017 at 16:10
Hello,
today I updated my Cube libraries to the last release and I found that in stm32f7xx_hal_can.c the HAL_UNLOCK is missing, in HAL_CAN_Receive_IT().
HAL_StatusTypeDef HAL_CAN_Receive_IT(CAN_HandleTypeDef* hcan, uint8_t FIFONumber)
{
/* Check the parameters */
assert_param(IS_CAN_FIFO(FIFONumber));
/* Check if CAN state is not busy for RX FIFO0 */
if((FIFONumber == CAN_FIFO0) && ((hcan->State == HAL_CAN_STATE_BUSY_RX0) || \
(hcan->State == HAL_CAN_STATE_BUSY_TX_RX0) || \
(hcan->State == HAL_CAN_STATE_BUSY_RX0_RX1) || \
(hcan->State == HAL_CAN_STATE_BUSY_TX_RX0_RX1)))
{
return HAL_BUSY;
}
/* Check if CAN state is not busy for RX FIFO1 */
if((FIFONumber == CAN_FIFO1) && ((hcan->State == HAL_CAN_STATE_BUSY_RX1) || \
(hcan->State == HAL_CAN_STATE_BUSY_TX_RX1) || \
(hcan->State == HAL_CAN_STATE_BUSY_RX0_RX1) || \
(hcan->State == HAL_CAN_STATE_BUSY_TX_RX0_RX1)))
{
return HAL_BUSY;
}
/* Process locked */
__HAL_LOCK(hcan);
/* Change CAN state */
if(FIFONumber == CAN_FIFO0)
{
switch(hcan->State)
{
case(HAL_CAN_STATE_BUSY_TX):
hcan->State = HAL_CAN_STATE_BUSY_TX_RX0;
break;
case(HAL_CAN_STATE_BUSY_RX1):
hcan->State = HAL_CAN_STATE_BUSY_RX0_RX1;
break;
case(HAL_CAN_STATE_BUSY_TX_RX1):
hcan->State = HAL_CAN_STATE_BUSY_TX_RX0_RX1;
break;
default: /* HAL_CAN_STATE_READY */
hcan->State = HAL_CAN_STATE_BUSY_RX0;
break;
}
}
else /* FIFONumber == CAN_FIFO1 */
{
switch(hcan->State)
{
case(HAL_CAN_STATE_BUSY_TX):
hcan->State = HAL_CAN_STATE_BUSY_TX_RX1;
break;
case(HAL_CAN_STATE_BUSY_RX0):
hcan->State = HAL_CAN_STATE_BUSY_RX0_RX1;
break;
case(HAL_CAN_STATE_BUSY_TX_RX0):
hcan->State = HAL_CAN_STATE_BUSY_TX_RX0_RX1;
break;
default: /* HAL_CAN_STATE_READY */
hcan->State = HAL_CAN_STATE_BUSY_RX1;
break;
}
}
/* Set CAN error code to none */
hcan->ErrorCode = HAL_CAN_ERROR_NONE;
/* Enable interrupts: */
/* - Enable Error warning Interrupt */
/* - Enable Error passive Interrupt */
/* - Enable Bus-off Interrupt */
/* - Enable Last error code Interrupt */
/* - Enable Error Interrupt */
/* - Enable Transmit mailbox empty Interrupt */
__HAL_CAN_ENABLE_IT(hcan, CAN_IT_EWG |
CAN_IT_EPV |
CAN_IT_BOF |
CAN_IT_LEC |
CAN_IT_ERR |
CAN_IT_TME);
if(FIFONumber == CAN_FIFO0)
{
/* Enable FIFO 0 overrun and message pending Interrupt */
__HAL_CAN_ENABLE_IT(hcan, CAN_IT_FOV0 | CAN_IT_FMP0);
}
else
{
/* Enable FIFO 1 overrun and message pending Interrupt */
__HAL_CAN_ENABLE_IT(hcan, CAN_IT_FOV1 | CAN_IT_FMP1);
}
__HAL_UNLOCK(hcan); // <------- THIS LINE WAS MISSING
/* Return function status */
return HAL_OK;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I added it (at line 1095 of the original file) and now everything works, apparently.
Best Regards,
Andrea
#bug #cube #f7 #can