Skip to main content
wjandsq
Associate II
Feb 13, 2026 1:17 PM UTC
Solved

CTS signal on USB CDC

To follow up this thread, CTS signal on USB CDC - STMicroelectronics Community

I'm experiencing a similar issue.

USBser.sys  have some problem

1. Only DTR Break can control alone

you can set  DTR is 1  or 0,  but  RTS have change,RTS only change with DTR.

2.  CDC Serial State

I  have test this code,  it  send from Endpoint 81h successfully,  but  PC USB Host  have no message

CDC_IN_Buf[0] = 0xA1; /* bmRequestType 0xA1 (10100001B) */
CDC_IN_Buf[1] = 0x20; /* 0x21 (SERIAL_STATE) */
CDC_IN_Buf[2] = 0x00; /* wValue LowByte */
CDC_IN_Buf[3] = 0x00; /* wValue HiByte */
CDC_IN_Buf[4] = 0x00; /* wIndex LowByte Default 0 */
CDC_IN_Buf[5] = 0x00; /* wIndex HiByte */
CDC_IN_Buf[6] = 0x02; /* wLength LowByte Serial State Length 0x0002 */
CDC_IN_Buf[7] = 0x00; /* wLength HiByte */
CDC_IN_Buf[8] = 0x14; /* Data LowByte */
CDC_IN_Buf[9] = 0x00; /* Data HiByte */
/*
CDC Serial State bit define (USB CDC 1.1 6.3.5 )
bit0 bRxCarrier 0x01
bit1 bTxCarrier 0x02
bit2 bBreak 0x04
bit3 bRingSignal 0x08
bit4 bFraming 0x10
bit5 bParity 0x20
bit6 bOverRun 0x40
*/
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, CDC_IN_Buf, 10);
USBD_LL_Transmit(&hUsbDeviceFS, CDC_CMD_EP, CDC_IN_Buf, 10);
 
Only CH341/FT232RL  can have  usb serial state notify ?
 
3.  Does ST have no technology? They can't write a single driver and can only use Microsoft's CDC driver。
 
 
FBLBest answer
ST Technical Moderator
Feb 18, 2026 9:40 AM UTC

Hi @wjandsq 

An internal ticket is submitted to dedicated team (227474) to check whether it's a bug. Would you provide more details about your HW setup and minimal project to reproduce the issue?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

14 replies

FBLBest answer
ST Technical Moderator
Feb 18, 2026 9:40 AM UTC

Hi @wjandsq 

An internal ticket is submitted to dedicated team (227474) to check whether it's a bug. Would you provide more details about your HW setup and minimal project to reproduce the issue?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
wjandsq
wjandsqAuthor
Associate II
Feb 20, 2026 2:09 PM UTC

you can set  DTR is 1  or 0,  but  RTS have no change,RTS only change with DTR.  this is a bug.  

ST Technical Moderator
Feb 20, 2026 2:22 PM UTC

Hi @wjandsq  Can you provide an example to reproduce the issue?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
gbm
Super User
Feb 18, 2026 12:03 PM UTC

Maybe there is some problem with the configuration descriptor.

Last time I checked, the CDC ACM notifications in my USB stack were correctly handled by Windows. The default Windows driver is greatly simplified with regard to notification data handling. I also observed the behavior you describe (RTS/DTR).

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Pavel A.
Mar 1, 2026 8:44 PM UTC

But is there a real use case/story for DTR & RTS, besides of compatibility with FTDI and CH341?  Millions of users seem to be happy with the Windows in-box driver. 

 

wjandsq
wjandsqAuthor
Associate II
Mar 2, 2026 4:20 AM UTC

Millions of users seem to be satisfied with Windows' built-in drivers, but I am not.

Current solutions:
1. Imitate CH340/CH341 devices by using CH340/CH341 drivers.
The current device imitation of CH340N works well and is more stable than the Microsoft CDC Driver. But there are still some problems:
Each packet is only 32 bytes, limiting speed. Authorization from the device manufacturer wch.cn has not been obtained, so it cannot be used compliantly.

2. Imitate FT232RL devices by using FT232RL drivers.
64-byte packets can be used, but it has not been successful yet, and authorization from the device manufacturer FTDI is also required.

3. Use a USB Composite Device, here being a Custom HID CDC_ACM device.
The current problem is:
Once USB FS (PA11 PA12) is in Composite mode, the macro USE_USBD_COMPOSITE is enabled.
Then the USB Device Library used for USB HS (PB14 PB15) also switches to Composite mode.
Therefore, USB FS and USB HS must be in the same Composite mode. The appearance of the macro USE_USBD_COMPOSITE in this USB Device Library is really unfriendly.

Pavel A.
Mar 2, 2026 4:45 AM UTC

Thank you for this additional information. So, do you want to use RTS/CTS for flow control? If yes, how these signals are set by the WCH and FT drivers?  Do you have host side software that uses RTS/CTS flow control and relies on specific serial drivers or vendor's library, or middleware such as the Qt library?

[ trying to understand if the same can be implemented in the usbser in backward-compatible way, so it won't break existing apps... ]

[ AI suggests to check how this is handled by the TinyUSB library. ]