Skip to main content
Max Rest
Associate II
March 8, 2019
Solved

CRITICAL: stm32h7xx_hal_tim_ex.h wrong defines

Dear STM,

please fix the defines in stm32h7xx_hal_tim_ex.h as at least TIM_TIMx_ETR are either empty or wrong, according to the datasheet. Here is a short example, _NOT_ stating all incorrect positions:

NOW, IN THE FILE stm32h7xx_hal_tim_ex.h in STM32Cube_FW_H7_V1.3.2 :

#define TIM_TIM5_ETR_GPIO (0x00000000) /* !< TIM5_ETR is connected to GPIO */
#define TIM_TIM5_ETR_SAI2_FSA (0x00000000) /* !< TIM5_ETR is connected to SAI2 FS_A */
#define TIM_TIM5_ETR_SAI2_FSB (0x00000000) /* !< TIM5_ETR is connected to SAI2 FS_B */

CORRECT, according to RM0433 Rev 5, p. 1686/3247

#define TIM_TIM5_ETR_GPIO (0x00000000) /* !< TIM5_ETR is connected to GPIO */
#define TIM_TIM5_ETR_SAI2_FSA (0x00001000) /* !< TIM5_ETR is connected to SAI2 FS_A */
#define TIM_TIM5_ETR_SAI2_FSB (0x00002000) /* !< TIM5_ETR is connected to SAI2 FS_B */

This is a critical bug.

Thanks,

Maximilian Rest

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
March 8, 2019

Hello Max,

thank you for reporting,

This bug is already fixed internally. It should be in a next release.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

2 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
March 8, 2019

Hello Max,

thank you for reporting,

This bug is already fixed internally. It should be in a next release.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Max Rest
Max RestAuthor
Associate II
March 8, 2019

Hi Mike,

thanks for your quick reply, sounds good. I hope you meant in _the_ next release though, because fixing it manually and overwriting it each time cube regenerates the files is quite ... annoying.

Best,

Max