Skip to main content
Visitor II
Dec 3, 2025 8:11 AM UTC
Question

Create Releases for STM32 Software published on Github

Hello,

This is a general suggestion that I would like to make. While I think it's great that all HAL libraries are available on GitHub, I would like to suggest creating a github release for the official versions in addition to creating tags. This can be done on GitHub with just a few clicks. The reason for this is the use of component analysis platforms such as Dependency Track, which make it possible to automatically track the libraries used, a task that is becoming increasingly important. Unfortunately, Dependency Track requires a release in order to track the version. While it is also possible to track this using the commit ID, for example, a release would be the better approach here. I welcome feedback and the possible realization of this suggestion.
For Example ARM is doing this with their CMSIS Package: https://github.com/ARM-software/CMSIS_5

-Hannes

1 reply

ST Technical Moderator
Dec 3, 2025 10:37 AM UTC

Hello @HannesD1 

Thanks for this suggestion and welcome to the community!

Unfortunately for the moment there is no plan to deploy this. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om