Skip to main content
clock.1166
Senior
Mar 14, 2024 5:34 PM UTC
Question

CORS with LWIP

Hi - can anyone tell me how to insert a CORS header into LWIP?

(Cross-Origin Resource Sharing) header directly into the httpd.c? file of LwIP)

i.e.Access-Control-Allow-Origin: *

I am using vscode to debug an index.shtml file file, but i need to get responses from my H743 webserver to be able to debug fully.

Any ideas?

Thanks

Chris

This topic has been closed for replies.

8 replies

Andrew Neil
Super User
Mar 14, 2024 5:47 PM UTC

From https://developer.mozilla.org/en-US/docs/Web/HTTP/CORS  it looks like they're just standard HTTP headers ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
clock.1166
Senior
Mar 15, 2024 9:54 AM UTC

Thanks Andrew,

Thats quite interesting - but I'm trying to find out where and how to insert these headers into the LWIP response CODE. I have found various places, but none of my attempts appear to work.

Unfortunately, I am not an expert in LWIP webserver code and I do not have weeks of time to spare!

Chris

 

Andrew Neil
Super User
Mar 15, 2024 10:16 AM UTC

neither am I.

But, given they're just ordinary HTTP headers, then inserting them should should be the as inserting any other headers?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
clock.1166
Senior
Mar 15, 2024 1:30 PM UTC

Apparently, you cant just add CORS headers directly to the HTML file.

I'm trying to find exactly where in the LWIP (perhaps httpd.c) code I can add them!

Andrew Neil
Super User
Mar 15, 2024 1:53 PM UTC

That doesn't sound right: HTTP is a transport protocol - HTML is a payload format.

:thinking_face:

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
clock.1166
Senior
Mar 15, 2024 2:36 PM UTC

From what I've deduced from searching, the way to dynamically add the CORS header into LWIP is somewhere in the httpd.c file.

But where and how?

Explorer
Mar 22, 2024 10:24 AM UTC

Hello!

I am facing the same problem! I think we need to add the CORS policy headers in this section: 

static const char *const g_psHTTPHeaderStrings[] = {
 "HTTP/1.0 200 OK\r\n",
 "HTTP/1.0 404 File not found\r\n",
 "HTTP/1.0 400 Bad Request\r\n",
 "HTTP/1.0 501 Not Implemented\r\n",
 "HTTP/1.1 200 OK\r\n",
 "HTTP/1.1 404 File not found\r\n",
 "HTTP/1.1 400 Bad Request\r\n",
 "HTTP/1.1 501 Not Implemented\r\n",
 "Content-Length: ",
 "Connection: Close\r\n",
 "Connection: keep-alive\r\n",
 "Connection: keep-alive\r\nContent-Length: ",
 "Server: "HTTPD_SERVER_AGENT"\r\n",
 // Add CORS headers
 "Access-Control-Allow-Origin: *\r\n",
 "Access-Control-Allow-Methods: GET, POST, OPTIONS\r\n",
 "Access-Control-Allow-Headers: Content-Type\r\n",
 "\r\n<html><body><h2>404: The requested file cannot be found.</h2></body></html>\r\n"
#if LWIP_HTTPD_SUPPORT_11_KEEPALIVE
 , "Connection: keep-alive\r\nContent-Length: 77\r\n\r\n<html><body><h2>404: The requested file cannot be found.</h2></body></html>\r\n"
#endif
};

But there is something missing.

Let me know if you find any solution.

clock.1166
Senior
Mar 22, 2024 10:37 AM UTC

Hi Jp - i've tried that already - makes no difference. I need to do a bit (lot) of studying!!

Good Luck!