Skip to main content
CTapp.1
Senior III
Mar 26, 2025 4:22 PM UTC
Solved

Conversion from 'int' to 'char' for use of return value from __io_getchar()

The compiler is correctly warning about an int to char conversion for the following code from syscalls.c:

extern int __io_getchar(void) __attribute__((weak));

...

__attribute__((weak)) int _read(int file, char *ptr, int len)
{
 (void)file;
 int DataIdx;

 for (DataIdx = 0; DataIdx < len; DataIdx++)
 {
 *ptr++ = __io_getchar(); // Warning here
 }

 return len;
}

Whilst the behaviour here is as intended (assuming EOF is not expected), the warning is a pain for any projects using -Wconversion.

Could this please be fixed by adding a cast?

*ptr++ = ( char )__io_getchar();

This is for an STM32G484CEUx device, if that's important.

This topic has been closed for replies.
Bob S
Bob SBest answer
Super User
Mar 26, 2025 9:41 PM UTC

You can make that change yourself.  The syscalls.c does not get re-generated every time you run CubeMX "generate code", so it won't overwrite your changes.

Though, yes, it would be nice if syscalls.c had lots simple mods to pass more strict compiler checks, like adding UNUSED() for the function parameters that are not used in the stub functions.

3 replies

Bob S
Bob SBest answer
Super User
Mar 26, 2025 9:41 PM UTC

You can make that change yourself.  The syscalls.c does not get re-generated every time you run CubeMX "generate code", so it won't overwrite your changes.

Though, yes, it would be nice if syscalls.c had lots simple mods to pass more strict compiler checks, like adding UNUSED() for the function parameters that are not used in the stub functions.

CTapp.1
CTapp.1Author
Senior III
Mar 27, 2025 9:04 AM UTC

Thanks, that will save me some "pain" - I hadn't spotted that those files aren't regenerated.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Bob S
Super User
Apr 2, 2025 5:37 PM UTC

How about flagging the post as "the answer" (please)