Skip to main content
Visitor II
Feb 21, 2025 7:26 AM UTC
Question

Connect to the multiple Cellular hardware

I'm working on an STM32 project using X-CUBE-CELLULAR to support both cellular modems: BG96 (or GM01Q). I physically connected both modems (2× STMod+ expansion connectors) to my STM32 board.

My main question is: How can I configure my project and steps to allow me to select and switch between controlling either the BG96 or the GM01Q modem at runtime using the X-CUBE-CELLULAR package?
If the package already supported, which configuration we should attend ?

This topic has been closed for replies.

1 reply

ST Technical Moderator
Mar 28, 2025 8:34 AM UTC

Hello @Alan5 

I reported your question internally and will get back to you as soon as possible.

Internal ticket number: 206379 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om