Skip to main content
MPera
Associate
September 11, 2019
Question

Confusion with interrupts and handlers in HAL

  • September 11, 2019
  • 1 reply
  • 769 views

I'm using stm32f103c6, i'm confused as to how should i handle the interrups, what i need is to count pulses from an external source, it has to be accurate so the best way is to do it with timers right? So i've configured the cnt_en from timer2 to act as trigger output for timer1 (gated mode), it will start counting until cnt_en goes down when timer2 reaches 1second (internal clock presscaller set to 36000-1 with the bus clock set to 36Mhz).

In the nvic tab i enabled:

-timer1: trigger and conmutation interrups and the update interrupt

-timer2: global interrupt

All this was done with cubeMx V4.27

My question is: what should i use to handle those interrupts? If i hover the mouse over the interrupt names in cubemx it shows the name if the interrupt handler, or what is it? For example i see for tim1:

HAL_TIM_IRQHandler

TIM1_TRG_COM_IRQn

TIM1_TRG_COM_IRQHandler

TIM1_TRG_COM_TIM11_IRQHandler

and for tim2: TIM2_IRQn

what i want to know is when tim2 ends so that i can stop it and get the count from timer1 and if timer1 overflows before the windows ends, with this i can reduce the time window or set the input prescaller for timer1 and try again.

Furthermore, i saw in stm32f1xx_hal_msp.c the function HAL_TIM_Base_MspInit

by it's content i assume that it sets the nvic and gpios etc, should it be called only once or every time i want to start the timer?

Sorry if this are basic questions, i searched a lot and asked my teachers (electronic engeneers, but they are useless).

Hope i explained myself correctly, as you may have already guessed, english is not my first language.

Attached is the timer init code generated by cubemx.

static void MX_TIM1_Init(void)
{
 
 TIM_ClockConfigTypeDef sClockSourceConfig;
 TIM_SlaveConfigTypeDef sSlaveConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 0xffff;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_ETRMODE2;
 sClockSourceConfig.ClockPolarity = TIM_CLOCKPOLARITY_NONINVERTED;
 sClockSourceConfig.ClockPrescaler = TIM_CLOCKPRESCALER_DIV1;
 sClockSourceConfig.ClockFilter = 0;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sSlaveConfig.SlaveMode = TIM_SLAVEMODE_GATED;
 sSlaveConfig.InputTrigger = TIM_TS_ITR1;
 if (HAL_TIM_SlaveConfigSynchronization(&htim1, &sSlaveConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
}
 
/* TIM2 init function */
static void MX_TIM2_Init(void)
{
 
 TIM_ClockConfigTypeDef sClockSourceConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 TIM_OC_InitTypeDef sConfigOC;
 
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 36000-1;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 0xffff;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
}

This topic has been closed for replies.

1 reply

S.Ma
Principal
September 11, 2019

Use the timer channel 1 or 2 to put your signal as the timer clock.

Start the counting from zero, wait 1 second, read the result.

If you don't need accuracy, you can probably run this by polling and no interrupt to get started.

Then just get the 1 second overflow to read the first edge counter timer and make a relative difference.