Skip to main content
Torsten_Robitzki
Associate
Nov 26, 2025 4:06 PM UTC
Solved

Confused by Run* state of STMH7 and the startup code that jumps to ExitRun0Mode

According to RM0433 Rev 8:

The Run* mode is entered after a POR reset and a wakeup from Standby. In Run*
mode, the performance is limited and the system supply configuration shall be
programmed in PWR control register 3 (PWR_CR3). The system enters Run
mode only when the ACTVOSRDY bit in PWR control status register 1
(PWR_CSR1) is set to 1.

and

As long as ACTVOSRDY indicates that voltage levels are invalid, the system is in
Run* mode, write accesses to the RAMs are not permitted and VOS shall not be
changed.

Now, the startup code first jumps (bl ExitRun0Mode) to the C function `ExitRun0Mode()` which probably might involves writes to stack.

Is this construct (calling a C function from ASM) just relying on the compiler not touching the stack or am I'm reading the docs wrongly?

best regards

Torsten

Saket_OmBest answer
ST Technical Moderator
Nov 28, 2025 1:43 PM UTC

Hello @Torsten_Robitzki 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 222757 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

11 replies

KnarfB
Super User
Nov 26, 2025 7:13 PM UTC

The bl instruction places the return address in the lr register. If ExitRun0Mode is a leaf function (does not call other functions), there is no need for the compiler to save lr on the stack, but just to generate a bx lr instruction for return. The current implementation is indeed a leaf function that just sets PWR->CR3 and waits for the PWR_CSR1_ACTVOSRDY condition. No need to touch the stack.

But, interestingly, when compiled in Debug configuration (-O0 optimization), it will use the stack for saving r7 (callers frame pointer):

08000434 <ExitRun0Mode>:
 8000434:	b480 	push	{r7}
 8000436:	af00 	add	r7, sp, #0
 8000438:	4b09 	ldr	r3, [pc, #36]	@ (8000460 <ExitRun0Mode+0x2c>)
 800043a:	68db 	ldr	r3, [r3, #12]
 800043c:	4a08 	ldr	r2, [pc, #32]	@ (8000460 <ExitRun0Mode+0x2c>)
 800043e:	f023 0302 	bic.w	r3, r3, #2
 8000442:	60d3 	str	r3, [r2, #12]
 8000444:	bf00 	nop
 8000446:	4b06 	ldr	r3, [pc, #24]	@ (8000460 <ExitRun0Mode+0x2c>)
 8000448:	685b 	ldr	r3, [r3, #4]
 800044a:	f403 5300 	and.w	r3, r3, #8192	@ 0x2000
 800044e:	2b00 	cmp	r3, #0
 8000450:	d0f9 	beq.n	8000446 <ExitRun0Mode+0x12>
 8000452:	bf00 	nop
 8000454:	bf00 	nop
 8000456:	46bd 	mov	sp, r7
 8000458:	f85d 7b04 	ldr.w	r7, [sp], #4
 800045c:	4770 	bx	lr
 800045e:	bf00 	nop
 8000460:	58024800 	.word	0x58024800

This is pointless as the caller is the startup code that does not use r7 at that time.

Hmm.

hth

KnarfB

Torsten_Robitzki
Associate
Nov 27, 2025 7:12 AM UTC

I think it's not surprising, that the compiler generate sub-optimal code without any optimization.

Do you think, I read the documentation correctly and the startup code is broken?

Bootloader off-the-shelf
KnarfB
Super User
Nov 27, 2025 11:10 AM UTC

No no surprise, but it looks like you found a bug.

I don't know the internals, but the cited RM explicitely forbids such access.

Maybe @mƎALLEm can help here.

As a quick workaround, you may add #pragma GCC optimize("O3") to the source code.

hth

KnarfB

 

Saket_OmBest answer
ST Technical Moderator
Nov 28, 2025 1:43 PM UTC

Hello @Torsten_Robitzki 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 222757 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Torsten_Robitzki
Associate
Nov 28, 2025 1:50 PM UTC

Thanks for taking the time to look into this.

Bootloader off-the-shelf