Skip to main content
Dave Nadler
Senior III
Dec 6, 2018 4:05 PM UTC
Solved

Confused about F413 flash programming and bootloader

We're looking at using the F413 for a slave in a many MCU product, and using its SPI bootloader so master can reprogram an array of slaves over SPI. I'm confused about the bootloader and flash programming, in particular:

(1) Is high voltage VPP and high current on BOOT0 pin required for any flash programming? Or only advantageous in some circumstance? Or can I just use 3.3v?

(2) datasheet says "parts are delivered with flash erased". So where is the bootloader? Do I need to avoid erasing the entire flash to preserve the bootloader? Or is it in ROM somewhere and mapped in only when BOOT0=1? Or is that Boot1=VPP?

Thanks in advance for any clarification!

Best Regards, Dave

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 6, 2018 5:46 PM UTC

It doesn't need VPP to work, pull-up BOOT0, or drive it high, to enter the System Loader, it will derive the power it needs from VDD.

The VPP option is to allow production test fixturing to more rapidly program the device. And why it should only be provided for a finite period.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Guru
Dec 6, 2018 4:09 PM UTC

The high VPP speeds programming/erase as the charge-pump doesn't need to generate the higher voltages internally.

The System Loader is in some OTP/ROM region, nominally in the 0x1FFxxxxx space. You aren't provided with means or opportunity to erase or modify it. The erase only relates to the user flash in the 0x080xxxxx space

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dave Nadler
Senior III
Dec 6, 2018 4:25 PM UTC

Thanks @Community member​ ! If I just use Vpp=3.3v to signal bootloader, do I need to provide high-current capability into BOOT0? or just any-old logic output will do?

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 6, 2018 5:46 PM UTC

It doesn't need VPP to work, pull-up BOOT0, or drive it high, to enter the System Loader, it will derive the power it needs from VDD.

The VPP option is to allow production test fixturing to more rapidly program the device. And why it should only be provided for a finite period.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dave Nadler
Senior III
Dec 6, 2018 11:05 PM UTC

So no high-current required. Thanks @Community member​ !