Skip to main content
path321
Associate II
Jan 15, 2025 1:19 PM UTC
Solved

Configure peripherals after sleep

Hi everyone,

During developing applications with STM32l476, using HSI16, I choose STOP1 or STOP2 mode to reduce power consumption , and wake up with RTC Alarm.

if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK) {
 Error_Handler();
}
HAL_SuspendTick();
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
//HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

Documentation states that RCC clocks (and most peripherals) are stopped during Stop mode, thus clock re-init is essential for proper wake up.


Do I have to also re-init peripherals used before entering Stop mode ? For example

//Not only
SystemClock_Config();
HAL_ResumeTick();

//But also
HAL_UART_Init(&htim3);
HAL_TIM_Base_Start_IT(&htim16);
...

 In the same spirit, do I have to De-Init peripherals before entering Stop mode ?
I have tested both init/DeInit and not, and both ways seem working, but is it safe to leave peripherals "as they were" before sleeping ? Is Init/Deinit for sleep "lost" cycles ?

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Jan 15, 2025 1:25 PM UTC

The datasheet should tell whether peripheral configs are retained during the various low-power modes?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

1 reply

Andrew Neil
Andrew NeilBest answer
Super User
Jan 15, 2025 1:25 PM UTC

The datasheet should tell whether peripheral configs are retained during the various low-power modes?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.