Skip to main content
Visitor II
Jun 17, 2024 12:08 PM UTC
Solved

Configure FatFs for 256 page size

Hello All,

 

 

I am planning to port FatFs on the IS25LP064A flash drive to communicate with my STM32H573ii over SPI. The FreeRTOS is running on STM32H573ii.

According to the IS25LP064A datasheet, the maximum page size is 256 bytes. The total size of the flash drive is 8 Mbyte.

1] Could you help me set the following parameters in FatFs?

GET_SECTOR_COUNT = 32768 (8 Mbyte / 256 bytes)

GET_SECTOR_SIZE = 256

Do I need to set the value of FF_MIN_SS since my maximum page size is 256 bytes?

FF_MIN_SS = 256

2] As per the datasheet, the erase block size is 4 Kbyte.

GET_BLOCK_SIZE = 16 (4 Kbyte / 256 bytes)

So Could you help me to find out the values of above parameters? Are they correct?

Thanks in advance.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 18, 2024 1:44 AM UTC

Use 4KB sectors, as this is your minimum erase size, write the sectors as 16 256-byte pages

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 18, 2024 1:44 AM UTC

Use 4KB sectors, as this is your minimum erase size, write the sectors as 16 256-byte pages

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..