Skip to main content
NathanWolcott
Associate III
Mar 17, 2021 9:27 PM UTC
Solved

Compile error for STM32G071RB Nucleo with UCPD and GUI interface enabled

While trying to test out the USB-PD middleware, I generated a project for the STM32G071RB Nulceo dev board with Tracer EMB and GUI interface enabled. Generating the code works fine however, I'm getting a compile error that traces back to the FLASH_SIZE macro in stm32g071xx.h

If I turn off the GUI module, the error goes away.

I was able to work around the problem by changing the FLASH_SIZE macro to just be the hard-coded size of the flash on my part, but this isn't a good solution.

The weird thing is, once I got the project to compile and load, I was able to past the original macro expression into the debugger expression evaluator and it came back with the correct answer (0x20000), so it doesn't seem to be a simple syntax error.

Here is the error:

In file included from ../Drivers/CMSIS/Device/ST/STM32G0xx/Include/stm32g0xx.h:117,
 from ../Core/Inc/usbpd_gui_memmap.h:31,
 from ../Utilities/GUI_INTERFACE/bsp_gui.h:23,
 from ../Utilities/GUI_INTERFACE/bsp_gui.c:22:
../Drivers/CMSIS/Device/ST/STM32G0xx/Include/stm32g071xx.h:640:34: error: operator '*' has no left operand
 640 | #define FLASH_SIZE (((*((uint32_t *)FLASHSIZE_BASE)) & (0x00FFU)) << 10U)
 | ^
../Drivers/STM32G0xx_HAL_Driver/Inc/stm32g0xx_hal_flash.h:889:42: note: in expansion of macro 'FLASH_SIZE'
 889 | #define FLASH_BANK_SIZE (FLASH_SIZE) /*!< FLASH Bank Size */
 | ^~~~~~~~~~
../Drivers/STM32G0xx_HAL_Driver/Inc/stm32g0xx_hal_flash.h:893:42: note: in expansion of macro 'FLASH_BANK_SIZE'
 893 | #define FLASH_PAGE_NB (FLASH_BANK_SIZE/FLASH_PAGE_SIZE) /* Number of pages per bank */
 | ^~~~~~~~~~~~~~~
../Core/Inc/usbpd_gui_memmap.h:55:34: note: in expansion of macro 'FLASH_PAGE_NB'
 55 | #define INDEX_PAGE (FLASH_PAGE_NB - 1u) /* Index of latest page */
 | ^~~~~~~~~~~~~
../Core/Inc/usbpd_gui_memmap.h:57:48: note: in expansion of macro 'INDEX_PAGE'
 57 | #define ADDR_FLASH_LAST_PAGE (FLASH_BASE + (INDEX_PAGE * FLASH_PAGE_SIZE)) /* Base @ of latest page */
 | ^~~~~~~~~~
../Core/Inc/usbpd_gui_memmap.h:60:40: note: in expansion of macro 'ADDR_FLASH_LAST_PAGE'
 60 | #define GUI_FLASH_MAGIC_NUMBER ADDR_FLASH_LAST_PAGE
 | ^~~~~~~~~~~~~~~~~~~~
../Utilities/GUI_INTERFACE/bsp_gui.c:24:5: note: in expansion of macro 'GUI_FLASH_MAGIC_NUMBER'
 24 | #if GUI_FLASH_MAGIC_NUMBER
 | ^~~~~~~~~~~~~~~~~~~~~~

Has anybody else seen this error?

This topic has been closed for replies.
Yohann M.
Yohann M.Best answer
ST Employee
Mar 18, 2021 6:57 AM UTC

Dear @NathanWolcott​ 

In the G0 package V1.4.0, this error should be linked to an issue in bsp_gui.c.

Please try to replace

#if GUI_FLASH_MAGIC_NUMBER

by

#if defined(GUI_FLASH_MAGIC_NUMBER)

Regards,

Yohann

5 replies

Yohann M.
Yohann M.Best answer
ST Employee
Mar 18, 2021 6:57 AM UTC

Dear @NathanWolcott​ 

In the G0 package V1.4.0, this error should be linked to an issue in bsp_gui.c.

Please try to replace

#if GUI_FLASH_MAGIC_NUMBER

by

#if defined(GUI_FLASH_MAGIC_NUMBER)

Regards,

Yohann

NathanWolcott
Associate III
Mar 18, 2021 3:43 PM UTC

Thanks Yohann!

I'm actually using G0 package V1.4.1 but apparently the problem is the same for both versions.

Your suggestion fixed the problem. I assume I will have to manually change these macros every time I regenerate the project?

Yohann M.
ST Employee
Mar 22, 2021 2:14 PM UTC

Dear @NathanWolcott​ 

This issue has been logged into our side. For sure, it will fix in next G0 maintenance release.

Btw, we just delivered a X-CUBE-TCPP V2.2.0 package under GitHub, which already includes this fix.

Feel free to have a look at this release!

Regards,

Yohann

NathanWolcott
Associate III
Mar 24, 2021 7:41 PM UTC

Hi @Yohann M.​ , I downloaded the new x-cube-tcpp package but I can't seem to find any instructions on how to install it. I tried to use the CubeMx import "from local" button in the software packages manager window but it gives an error that it doesn't recognize the package. I guess it's a stupid question, but how am I supposed to use this package with cubeIDE/cubeMX?

Thanks,

Nathan

Yohann M.
ST Employee
Mar 25, 2021 6:47 AM UTC

Hi @NathanWolcott​ 

This package is not part of the X-CUBE package downloaded directly through CubeMX.

You should open directly IOC files provided in each USB-PD application like:

https://github.com/STMicroelectronics/x-cube-tcpp/blob/main/Projects/NUCLEO-G071RB/Applications/USB_PD/SNK1M1_Sink/SNK1M1_Sink.ioc

When you open it CubeMX, you should see that it is linked to your package you uploader on your laptop like this:

0693W000008xrRAQAY.jpg 

Regards,

Yohann