Skip to main content
Senior III
October 23, 2025
Solved

CMSIS-DSP rfft init throwing an error

  • October 23, 2025
  • 2 replies
  • 258 views

STM32WB55

arm_rfft_fast_instance_f32 fft_instance;
arm_rfft_fast_init_f32(&fft_instance, NUM_SAMP);


I'm trying to use the rfft_fast function from the arm_math.h library

But when I compile I get...

 

../STM32_WPAN/App/custom_app.c:122:24: error: expected declaration specifiers or '...' before '&' token
122 | arm_rfft_fast_init_f32(&fft_instance, NUM_SAMP);
| ^
../STM32_WPAN/App/custom_app.c:69:25: error: expected declaration specifiers or '...' before numeric constant
69 | #define NUM_SAMP 256

 

I looked at the docs & many examples of the init function, the usage is always as above. Compiles fine if I comment out the init function but obviously that is of no use to me.

 

Best answer by TDK

You can't call functions directly like this at the global scope. This needs to be within a function such as main().

If that's not it, include the full custom_app.c file that throws this error.

2 replies

TDK
TDKBest answer
October 23, 2025

You can't call functions directly like this at the global scope. This needs to be within a function such as main().

If that's not it, include the full custom_app.c file that throws this error.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Senior III
October 23, 2025

Thanks, getting lost in my own code here...