Skip to main content
Visitor II
Feb 20, 2024 11:11 AM UTC
Question

CMSIS arm_biuad_cascade_df2T, filter coefficients degrade the signal

Hey everyone, i'm trying to implement CMSIS filtering function to my project. Sound sounds fine when i'm using 1,0,0,0,0 coeefs, but every single change makes filter degrading input signal, and i'm getting so much noise on output. I'm using coeffs from biquad calculator v3, witch was fine when i used eqation implementation with my own, but using CMSIS it don't wanna work. I remembered changing the sign in a1 and a2 coeffs. Here's my code, maybe someone will have any idea what's wrong:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "arm_math.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

I2S_HandleTypeDef hi2s1;
DMA_HandleTypeDef hdma_spi1_rx;
DMA_HandleTypeDef hdma_spi1_tx;

/* USER CODE BEGIN PV */
volatile static uint16_t adc_val[2];
float32_t rxBuf[1024];
float32_t txBuf[1024];
float32_t l_buf_in[256];
float32_t r_buf_in[256];
float32_t l_buf_out[256];
float32_t r_buf_out[256];

float32_t iir_coeffs[5] = { 1, 0, 0, 0, 0 };

float32_t iir_state[2];

uint16_t a, b = 0;

uint8_t callback_state = 0;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_I2S1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_I2S1_Init();
 /* USER CODE BEGIN 2 */
	arm_biquad_cascade_df2T_instance_f32 iir;
	arm_biquad_cascade_df2T_init_f32(&iir, 1, &iir_coeffs[0], &iir_state[0]);

	if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY,
	ADC_SINGLE_ENDED) != HAL_OK) {
		Error_Handler();
	}
	if (HAL_ADC_Start_DMA(&hadc1, (uint32_t*) adc_val, 2) != HAL_OK) {
		Error_Handler();
	}

	if (HAL_I2SEx_TransmitReceive_DMA(&hi2s1, (uint16_t*) txBuf,
			(uint16_t*) rxBuf, 1024) != HAL_OK) {
		Error_Handler();
	}
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
	while (1) {
		if (callback_state != 0) {
			if (callback_state == 1) {
				b = 0;
			} else if (callback_state == 2) {
				b = 512;
			}
			for (int i = b; i < b + 511; i = i + 2) {
				l_buf_in[a] = rxBuf[i];
				r_buf_in[a] = rxBuf[i + 1];
				a++;
			}
			a = 0;
			arm_biquad_cascade_df2T_f32(&iir, l_buf_in, l_buf_out, 256);
			arm_biquad_cascade_df2T_f32(&iir, r_buf_in, r_buf_out, 256);
			if (callback_state == 1) {
				b = 0;
			} else if (callback_state == 2) {
				b = 512;
			}
			for (int i = b; i < b + 511; i = i + 2) {
				txBuf[i] = l_buf_out[a];
				txBuf[i + 1] = r_buf_out[a];
				a++;
			}
			a = 0;
			callback_state = 0;
		}

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	}
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = 64;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 34;
 RCC_OscInitStruct.PLL.PLLP = 1;
 RCC_OscInitStruct.PLL.PLLQ = 3;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 3072;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_16B;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.OversamplingMode = ENABLE;
 hadc1.Init.Oversampling.Ratio = 16;
 hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_4;
 hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
 hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_CONTINUED_MODE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_16;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief I2S1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2S1_Init(void)
{

 /* USER CODE BEGIN I2S1_Init 0 */

 /* USER CODE END I2S1_Init 0 */

 /* USER CODE BEGIN I2S1_Init 1 */

 /* USER CODE END I2S1_Init 1 */
 hi2s1.Instance = SPI1;
 hi2s1.Init.Mode = I2S_MODE_MASTER_FULLDUPLEX;
 hi2s1.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s1.Init.DataFormat = I2S_DATAFORMAT_24B;
 hi2s1.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s1.Init.AudioFreq = I2S_AUDIOFREQ_48K;
 hi2s1.Init.CPOL = I2S_CPOL_LOW;
 hi2s1.Init.FirstBit = I2S_FIRSTBIT_MSB;
 hi2s1.Init.WSInversion = I2S_WS_INVERSION_DISABLE;
 hi2s1.Init.Data24BitAlignment = I2S_DATA_24BIT_ALIGNMENT_RIGHT;
 hi2s1.Init.MasterKeepIOState = I2S_MASTER_KEEP_IO_STATE_DISABLE;
 if (HAL_I2S_Init(&hi2s1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2S1_Init 2 */

 /* USER CODE END I2S1_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);
 /* DMA1_Stream1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
 /* DMA1_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_I2SEx_TxRxHalfCpltCallback(I2S_HandleTypeDef *hi2s) {

	callback_state = 1;

}

void HAL_I2SEx_TxRxCpltCallback(I2S_HandleTypeDef *hi2s) {

	callback_state = 2;

}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
	/* User can add his own implementation to report the HAL error return state */
	__disable_irq();
	while (1) {
	}
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
This topic has been closed for replies.