Skip to main content
Associate II
Jan 14, 2025 3:41 PM UTC
Question

Check on wake up reason after interrupt by RTC timer or interrupt pin

I do have problem to check wake up flag after wake-up from RTC timer or interrupt pin. This is my code block to check flag after wake-up:

 

 

void InitiateMode(int timeValue)
{
 turnOffPeripherals();
 timeValue = getTimeValue(timeValue);
 printf("\ngetMilSecBInSecond : %d\ntimeValue : %d\n\n", getMilSecBInSecond(), timeValue);
 HAL_SuspendTick();
 HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, timeValue, RTC_WAKEUPCLOCK_CK_SPRE_16BITS);

 printf("Boot : ");
 printf("%d\n", bootCount);
 printf("Sleep mode Start\n");
 printf("Enable deep sleep, Will wake up in %d seconds\n\n", timeValue);

 /* Enter STOP 2 mode */
 // HAL_PWREx_EnterSTOP0Mode(PWR_STOPENTRY_WFI);
 // HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

 getTotalTime();
 // betol2 sebelom
 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
 printf(" 2\n");

 // Check RTC Wake-Up Timer Flag
 if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) != RESET)
 {
 // Wake-up event detected, clear the flag
 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);

 // Your code to turn on the LED or perform other actions
 printf("Wake-up event detected by RTC timer, clear the flag\n");
 }
 if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) != RESET)
 {
 // Wake-up event detected, clear the flag
 __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7);

 // Your code to turn on the LED or perform other actions
 printf("Wake-up event detected by interrupt pin, clear the flag\n");
 }


 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

 SystemClock_Config();
 // processable start hidup sini
 // printf("\nBetol 2 lepas wake up : %d\n", HAL_GetTick());
 printf("\nBetol 2 lepas wake up : %lu\n", HAL_GetTick());
 HAL_ResumeTick();
 getTickTimeStart();

 printf("Sleep mode End\n");
 printf("Wake Up!!\n");
 printf("----------------------------------------------------------------\n\n");

 // Increment the bootCount
 ++bootCount;
 printf("Bootcount : %d\n", bootCount);
}

 

The section:

 

 // Check RTC Wake-Up Timer Flag
 if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) != RESET)
 {
 // Wake-up event detected, clear the flag
 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);

 // Your code to turn on the LED or perform other actions
 printf("Wake-up event detected by RTC timer, clear the flag\n");
 }
 // Check GPIO 7 interrupt pin Flag
 if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) != RESET)
 {
 // Wake-up event detected, clear the flag
 __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7);

 // Your code to turn on the LED or perform other actions
 printf("Wake-up event detected by interrupt pin, clear the flag\n");
 }

 

I set 10 second timer during STOP2 mode, after that the system wake-up, but when i check the log, no line is printed mean that __HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) == RESET or __HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_7) == RESET, is there any problem in my code? please help me sifu, i am already struck by lighting

 

This topic has been closed for replies.

3 replies

ST Employee
Jan 15, 2025 9:09 AM UTC

Hello @hlmn7, 

Could you check the initial state of flags before entering stop2 mode?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hlmn7Author
Associate II
Jan 21, 2025 3:33 AM UTC

Hi @Sarra.S, please check my latest reply. Thanks.

hlmn7Author
Associate II
Jan 15, 2025 2:18 PM UTC

Thanks for the reply, I just checked the initial state with the code added in void InitiateMode below:

 // Check RTC Wake-Up Timer Flag
 if (__HAL_RTC_WAKEUPTIMER_GET_FLAG(&hrtc, RTC_FLAG_WUTF) == SET)
 {
 // Your code to turn on the LED or perform other actions
 printf("Wake-up RTC timer flag is SET\n");
 } else {
 printf("Wake-up RTC timer flag is RESET\n");
 }

 // Check GPIO 7 interrupt pin Flag
 if (__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_7) == SET)
 {
 // Your code to turn on the LED or perform other actions
 printf("Interrupt GPIO_PIN_7 flag is SET\n");
 } else {
 printf("Interrupt GPIO_PIN_7 flag is RESET\n");
 }

the output:

22:12:22:545 -> Total time process : 6119
22:12:22:545 -> Wake-up RTC timer flag is RESET
22:12:22:545 -> Interrupt GPIO_PIN_7 flag is RESET

both are in reset state like I taught on top of the topic, I have no idea what to do next, I really need help on this.
@Sarra.S