Skip to main content
JSzem.1
Associate II
April 18, 2020
Question

CH1 insted of CH3 in TIM_PWMOutput Example_LL

  • April 18, 2020
  • 1 reply
  • 532 views

There is a bug in CubeH7 examples.

Folder: STM32Cube_FW_H7_V1.7.0\Projects\NUCLEO-H7A3ZI-Q\Examples_LL\TIM\TIM_PWMOutput

File: main.c

Funkcion: TimerCaptureCompare_Callback()

Instead of "if (LL_TIM_OC_GetCompareCH1(TIM3) > ARR )" should be "if (LL_TIM_OC_GetCompareCH3(TIM3) > ARR )".

Second bug in the same project:

In File stm32h7xx_it.c there is a comment in void TIM3_IRQHandler(void)

"/* Check whether CC1 interrupt is pending */". It slould be "/* Check whether CC3 interrupt is pending */"

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 21, 2020

Hello @JSzem.1​ ,

Thank you for your contribution and highlighting this issue.

I raised this internally for correction in the coming release of STM32CubeH7 firmware package.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks