Skip to main content
Associate II
March 1, 2017
Question

capture and play sound by STM32F407 and Codec

  • March 1, 2017
  • 0 replies
  • 814 views
Posted on March 01, 2017 at 10:34

Hi.

I designed a PCB to use stm32f407 and TLV320AIC12 codec for capturing and playing sound.

As you can see I connected I2S pin of stm to tlv in this way:

STM32F407                   TLV320AIC12

CK---------------------------->SCLK

WS--------------------------->FS

ext_SD---------------------->Dout

SD---------------------------->Din

MCK-------------------------->MCLK

and also I connected INP to microphone and OUTP1 to speaker.

I used stmcube software for configure my application, so I wrote my code in the following format and started speaking in microphone but I could not hear any voice from speaker.

I do not have any idea why it is not working.

thank you for guiding me in advance.

//*******************************************************************

        MX_I2S2_Init();

        uint8_t CnvRx[50];

        uint16_t Txbuff[5];

        uint16_t Rxbuff[5];

        while(1)

        {

            Txbuff[0]=Rxbuff[0]; //DAC input data

            Txbuff[1]=0x0000;

            HAL_I2SEx_TransmitReceive(&hi2s2,Txbuff,Rxbuff,2,100);

            sprintf((char*)CnvRx,'%04X,%04X\n',Rxbuff[0],Rxbuff[1]);

            Debugger_Send_Data(CnvRx);//send data out by uart

        }

 DebuggerOutput:

000F,0000

0010,0000

000D,8000

000E,0000

000E,8000

//*******************************************************************

#stm32f407 #tlv320aic12 #codec
This topic has been closed for replies.