Can you kindly help me to get system bootloader working?
Im my system based on STM32H753 I would like to use system bootloader by USART1.
After struggling with my PCB without getting bootloader working then I switched to NUCLEO-H743ZI2 board.
From AN2606 I know that PA10 is RX input and PA9 is TX output so I connected the PC by an USB to 3V3 TTL converter accordingly in CN12.
From NUCLEO schematic I saw that PA9/PA10 are connected to USB_FS signals and so I removed SB23 / SB24 jumpers to isolate them.
The STM32H74xxx/75xxx bootloader is activated by applying pattern10; in my case
Boot(pin) = 1 and BOOT_ADD1(optionbyte) = 0x1FF0 (checked by STM32 ST-LINK Utility -> target -> option bytes)
So I connected BOOT0 pin to 3V3 and power by plugging USB in CN1.
Then I used FLASHER-STM32 demostrator pointed to the COM port of the converter.
The program report always "no response from the target...".
I checked the PA10/PA9 signals and I found that are at 3V3; just when I run the demostrator I saw 2 low going pulses on PA10.
Both pulses are around 8.7us and are separate by 60.8us. This should be 0x7F at 115200,8,E,1 (as written in AN3155).
I tried also other lower speeds.
Is there anyone who can suggest what I'm doing wrong?
Thank you
Ciao
Marco