Skip to main content
ABhat.7
Associate III
May 21, 2021 4:06 PM UTC
Question

Can we combine hal based project with register level project

Hi, everyone

​

I have 2 project in one of the project i have used hal library for stm32f1 while in the other project i have use register access i.e all the peripheral like uart, adc are accessed at register level ​like in stm8 pls suggest is it possible to merge these 2 project

​

​

This topic has been closed for replies.

3 replies

TDK
May 21, 2021 10:32 PM UTC

There are no issues in general combining HAL and register level access, but generally you should only use HAL or register level access for a particular peripheral. The only problem comes from using both for the same peripheral without understanding how HAL operates and how accessing registers affects it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ABhat.7
ABhat.7Author
Associate III
May 22, 2021 1:37 AM UTC

Hi ,@[TDK]​

​

Thank for reply but can you provide any examples or links through which i can get reference that how to merge them ​

TDK
May 22, 2021 1:55 AM UTC
Not sure what you're looking for. Copy the relevant code from one project to the other and adjust programming logic according to how you want them to be used. If they don't interact with one another, it should be a straightforward task.
"If you feel a post has answered your question, please click ""Accept as Solution""."