Question
Can USB HS be used when VDD is 1V8 with an external ULPI PHY on STM32H750VBT6?
I understand that VDD needs to be 3V3 if using the internal full speed transceiver, since STM32H750VBT6 has no VDDUSB input, but if I am using an external high speed USB ULPI PHY can the mcu be run at 1V8 and still use USB? I wan't quite able to figure out from the datasheet.
Thanks,
Jacob