Skip to main content
Associate III
Jan 16, 2025 7:01 AM UTC
Solved

CAN Transmit mailbox callback function understanding

Hi

My board is STM32F407G so I want to understand the tx mailbox callback once interrupt hit I am sharing project in which I am sending CAN1 to CAN2 and CAN2 to CAN1 in loop back mode same ID.

So rxindication is working fine and this is the project I got from one of your technical executive  ,so how will "hcan->TxMailbox0CompleteCallback(hcan);" get called because in above line we are clearing "

/* Clear the Transmission Complete flag (and TXOK0,ALST0,TERR0 bits) */

__HAL_CAN_CLEAR_FLAG(hcan, CAN_FLAG_RQCP0);"

which also clears "if ((tsrflags & CAN_TSR_TXOK0) != 0U)" TXOK0 bit also so if condition will not satisfy . please guide me 

 

/* Transmit Mailbox empty interrupt management *****************************/

if ((interrupts & CAN_IT_TX_MAILBOX_EMPTY) != 0U)

{

/* Transmit Mailbox 0 management *****************************************/

if ((tsrflags & CAN_TSR_RQCP0) != 0U)

{

/* Clear the Transmission Complete flag (and TXOK0,ALST0,TERR0 bits) */

__HAL_CAN_CLEAR_FLAG(hcan, CAN_FLAG_RQCP0);



if ((tsrflags & CAN_TSR_TXOK0) != 0U)

{

/* Transmission Mailbox 0 complete callback */

#if USE_HAL_CAN_REGISTER_CALLBACKS == 1

/* Call registered callback*/

hcan->TxMailbox0CompleteCallback(hcan);

#else

/* Call weak (surcharged) callback */

HAL_CAN_TxMailbox0CompleteCallback(hcan);

#endif /* USE_HAL_CAN_REGISTER_CALLBACKS */

}

 

 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1;
CAN_HandleTypeDef hcan2;

/* USER CODE BEGIN PV */
CAN_FilterTypeDef sFilterConfig;
__IO uint32_t i = 0;
// CAN1
CAN_TxHeaderTypeDef CAN1_TxHeader;
CAN_RxHeaderTypeDef CAN1_RxHeader[9];
uint8_t CAN1_TxData[2] = {0};
uint8_t CAN1_RxData[2] = {0};
uint32_t CAN1_TxMailbox;
uint32_t CAN1_Tx_ID_List[3] = {0x501,0x502,0x503};
__IO uint8_t CAN1_Rx_cnt = 0;
// CAN2
CAN_TxHeaderTypeDef CAN2_TxHeader;
CAN_RxHeaderTypeDef CAN2_RxHeader[9];
uint8_t CAN2_TxData[2] = {0};
uint8_t CAN2_RxData[2] = {0};
uint32_t CAN2_TxMailbox;
uint32_t CAN2_Tx_ID_List[3] = {0x501,0x502,0x503};
__IO uint8_t CAN2_Rx_cnt = 0;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN1_Init(void);
static void MX_CAN2_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_CAN1_Init();
 MX_CAN2_Init();
 /* USER CODE BEGIN 2 */
 sFilterConfig.FilterBank = 0;
 sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
 sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
 sFilterConfig.FilterIdHigh = 0x0000;
 sFilterConfig.FilterIdLow = 0x0000;
 sFilterConfig.FilterMaskIdHigh = 0x0000;
 sFilterConfig.FilterMaskIdLow = 0x0000;
 sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 sFilterConfig.FilterActivation = ENABLE;
 sFilterConfig.SlaveStartFilterBank = 1;
 
 if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
 {
 /* Filter configuration Error */
 Error_Handler();
 }
 
 sFilterConfig.FilterBank = 1;
 sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
 sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
 sFilterConfig.FilterIdHigh = 0x0000;
 sFilterConfig.FilterIdLow = 0x0000;
 sFilterConfig.FilterMaskIdHigh = 0x0000;
 sFilterConfig.FilterMaskIdLow = 0x0000;
 sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 sFilterConfig.FilterActivation = ENABLE;
 sFilterConfig.SlaveStartFilterBank = 1;
 
 if(HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig) != HAL_OK)
 {
 /* Filter configuration Error */
 Error_Handler();
 } 
 
 if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
 {
 /* Notification Error */
 Error_Handler();
 } 
 
 if (HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
 {
 /* Notification Error */
 Error_Handler();
 } 
 
 CAN1_TxHeader.ExtId = CAN2_TxHeader.ExtId = 0x01;
 CAN1_TxHeader.RTR = CAN2_TxHeader.RTR = CAN_RTR_DATA;
 CAN1_TxHeader.IDE = CAN2_TxHeader.IDE = CAN_ID_STD;
 CAN1_TxHeader.DLC = CAN2_TxHeader.DLC = 2;
 CAN1_TxHeader.TransmitGlobalTime = CAN2_TxHeader.TransmitGlobalTime = DISABLE;
 
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 CAN1_TxHeader.StdId = CAN1_Tx_ID_List[i];
 CAN1_TxData[0] ++;
 CAN1_TxData[1] --;
 if (HAL_CAN_AddTxMessage(&hcan1, &CAN1_TxHeader, CAN1_TxData, &CAN1_TxMailbox) != HAL_OK)
 {
 /* Transmission request Error */
 Error_Handler();
 }
 HAL_Delay(10); 
 
 CAN2_TxHeader.StdId = CAN2_Tx_ID_List[i];
 if (HAL_CAN_AddTxMessage(&hcan2, &CAN2_TxHeader, CAN2_TxData, &CAN2_TxMailbox) != HAL_OK)
 {
 /* Transmission request Error */
 Error_Handler();
 }
 HAL_Delay(10); 
 i++;
 if (i == 3) i = 0; 

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief CAN1 Initialization Function
 * None
 * @retval None
 */
static void MX_CAN1_Init(void)
{

 /* USER CODE BEGIN CAN1_Init 0 */

 /* USER CODE END CAN1_Init 0 */

 /* USER CODE BEGIN CAN1_Init 1 */

 /* USER CODE END CAN1_Init 1 */
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 4;
 hcan1.Init.Mode = CAN_MODE_LOOPBACK;
 hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_15TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_5TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = DISABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CAN1_Init 2 */
 if (HAL_CAN_Start(&hcan1) != HAL_OK)
 {
 /* Start Error */
 Error_Handler();
 }
 /* USER CODE END CAN1_Init 2 */

}

/**
 * @brief CAN2 Initialization Function
 * None
 * @retval None
 */
static void MX_CAN2_Init(void)
{

 /* USER CODE BEGIN CAN2_Init 0 */

 /* USER CODE END CAN2_Init 0 */

 /* USER CODE BEGIN CAN2_Init 1 */

 /* USER CODE END CAN2_Init 1 */
 hcan2.Instance = CAN2;
 hcan2.Init.Prescaler = 4;
 hcan2.Init.Mode = CAN_MODE_LOOPBACK;
 hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan2.Init.TimeSeg1 = CAN_BS1_15TQ;
 hcan2.Init.TimeSeg2 = CAN_BS2_5TQ;
 hcan2.Init.TimeTriggeredMode = DISABLE;
 hcan2.Init.AutoBusOff = DISABLE;
 hcan2.Init.AutoWakeUp = DISABLE;
 hcan2.Init.AutoRetransmission = DISABLE;
 hcan2.Init.ReceiveFifoLocked = DISABLE;
 hcan2.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CAN2_Init 2 */
 if (HAL_CAN_Start(&hcan2) != HAL_OK)
 {
 /* Start Error */
 Error_Handler();
 }
 /* USER CODE END CAN2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
 /* Get RX message */
 if(hcan->Instance == CAN1)
 {
 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &CAN1_RxHeader[CAN1_Rx_cnt++], CAN1_RxData) != HAL_OK)
 {
 /* Reception Error */
 Error_Handler();
 }
 
 if(CAN1_Rx_cnt == 9) CAN1_Rx_cnt = 0;
 }
 else if(hcan->Instance == CAN2) 
 {
 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &CAN2_RxHeader[CAN2_Rx_cnt++], CAN2_RxData) != HAL_OK)
 {
 /* Reception Error */
 Error_Handler();
 }
 if(CAN2_Rx_cnt == 9) CAN2_Rx_cnt = 0;
 } 

}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 20, 2025 9:46 AM UTC

Hello,

Not sure I understood the issue.

In your attached example you didn't activate the Tx empty interrupt with no Tx callback declared. How do you expect to get Tx callback called?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

Ash1Author
Associate III
Jan 20, 2025 5:18 AM UTC

Hi all

Still I haven't received any response related this.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 20, 2025 9:46 AM UTC

Hello,

Not sure I understood the issue.

In your attached example you didn't activate the Tx empty interrupt with no Tx callback declared. How do you expect to get Tx callback called?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.