Skip to main content
chriscole
Associate II
Jul 6, 2022 3:24 PM UTC
Question

Can the ROM bootloader in the STM32H7 be configured to use the high speed USB interface instead of the full speed USB interface?

..

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jul 6, 2022 3:51 PM UTC

It can do only what's indicated in the AN2606 app note.

The high-speed modes typically use an external PHY, adding to the complexity.

Generally the ROM is designed to handle a sub-set of functionality to provide a limp-home type recovery mode/method that's only dependent on what's within the chip, and not dependent on external circuitry and board level complexity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..