Skip to main content
Mikk Leini
Senior
Feb 12, 2026 7:47 AM UTC
Question

Can't use STM32N6 DCMIPP continuous mode after snapshot mode

There's a bug in STM32N6 HAL DCMIPP driver function DCMIPP_SetConfig.

It only sets capture mode bits for PIPE0 to PIPE2, but does not clear them:

 /* Set the capture mode */
 hdcmipp->Instance->P0FCTCR |= CaptureMode;

CaptureMode options are:

#define DCMIPP_MODE_CONTINUOUS 0U /*!< DCMIPP continuous mode (preview) */
#define DCMIPP_MODE_SNAPSHOT DCMIPP_P0FCTCR_CPTMODE /*!< DCMIPP snapshot mode */

As a result, after having DCMIPP in snapshot mode it is not possible to re-configure DCMIPP into continuous mode using HAL.

Workaround is to manually clear CPTMODE bit.

1 reply

ST Technical Moderator
Feb 24, 2026 8:43 AM UTC

Hello @Mikk Leini 

The issue has been resolved internally and will be released as soon as possible. 

Internal ticket number: 220344 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om