Skip to main content
ACaso.1
Visitor II
Jun 30, 2021 9:25 AM UTC
Question

Can't read Flash size data register from uart bootloader with micro STM32L4

Following the "RM0394 Reference manual", I'm trying to read the "Flash size data register" using the Base address: 0x1FFF 75E0 with the USART protocol (serial) but i receive the NACK response.

I see in the Memory Map of the "RM0394 Reference manual" that the address 0x1FFF 75E0 is in a RESERVED space, so i realize can't read the "Flash size" and the "device uid" through the bootloader USART protocol.

Is there some other way to get it?

I'm using a Chip ID: 0x435 wit BootLoader protocol version: 3.1

This topic has been closed for replies.