Skip to main content
Associate
Feb 14, 2025 3:12 AM UTC
Solved

Can't Get Blinky Project working With FreeRTOS

I am new to FreeRTOS ( RTOS in general, although I am very familiar with baremetal) and am following along with this video:https://www.youtube.com/watch?v=CdpgqpuPSyQ&t=4s 

I am using a STM32F3DISCOVERY board so I had to make some minor tweaks to follow along, seemingly just pin numbering. I am using the default pin configurations and clock configuration. I am using TIM6 as Timebase source. I cannot seem to figure out why my LEDs are not blinking. I created a baremetal project to confirm the config of the pins is good and there I can get them toggling. I see the TIM6 CNT incrementing and wrapping so that is working. I tried to use breakpoints to see if I ever get back to my task and aside from the first hit during initialization, I never get back.

Not sure what I did wrong, but it appears my tasks only occur once and then terminate but I cannot figure out why. Any tips on how to debug this? Thank you

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 6, 2025 8:09 AM UTC

Issue fixed in CubeMx 6.14.0 (already available on ST website)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

11 replies

KnarfB
Super User
Feb 14, 2025 5:07 AM UTC

> I am using TIM6 as Timebase

in main.c, there is no reference to TIM6, but TIM4. 

hth

KnarfB

Associate
Feb 14, 2025 5:13 AM UTC

I used TIM6 originally like the demo but after some debugging effort I played around with trying others, meant to change it back to TIM6 before uploading that is my mistake. I do not believe it is the issue however

KnarfB
Super User
Feb 14, 2025 6:26 AM UTC

>  I do not believe 

seeing is believing.

Set a breakpoint at the timer callback and check that it is called. The interrupt handler is in the *_it.c file. Check that everything is consistent.

hth

KnarfB

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 6, 2025 8:09 AM UTC

Issue fixed in CubeMx 6.14.0 (already available on ST website)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.