Skip to main content
Visitor II
Oct 10, 2024 2:42 PM UTC
Question

Calculating Flash data CRC using DMA

I am currently working on calculating the FLASH CRC through DMA on the NUCLEO-H755ZI-Q development board. I've successfully read from flash and calculated the CRC using DMA in memory-to-memory.

Now, I'm facing challenges while configuring DMA for DMA_MEMORY_TO_PERIPH. I attempted to read directly from flash into the CRC register using the following call:

" HAL_DMA_Start(&hdma_dma_generator0, (uint32_t)flash_start_addr, (uint32_t)&CRC->DR, FLASH_BUFFER_SIZE); "
Is it feasible to calculate the CRC using DMA_MEMORY_TO_PERIPH? I would appreciate any suggestions or insights you might have!

Here are my current DMA configurations:
hdma_dma_generator0.Instance = DMA1_Stream0;
hdma_dma_generator0.Init.Request = DMA_REQUEST_GENERATOR0;
hdma_dma_generator0.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_dma_generator0.Init.PeriphInc = DMA_PINC_ENABLE;
hdma_dma_generator0.Init.MemInc = DMA_MINC_ENABLE;
hdma_dma_generator0.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_dma_generator0.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_dma_generator0.Init.Mode = DMA_NORMAL;
hdma_dma_generator0.Init.Priority = DMA_PRIORITY_HIGH;
hdma_dma_generator0.Init.FIFOMode = DMA_FIFOMODE_DISABLE;


Thank you for your help!

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Oct 10, 2024 3:00 PM UTC

Use "memory to memory".

Don't let the "peripheral" and/or "memory" confuse you, it is (mostly) not about physical memory or peripheral, but about the way how DMA is triggered. In M2M transfers, DMA is triggered automatically by DMA itself and performs all transfers at once. Other transfers require some peripheral to trigger them.

JW

ST Technical Moderator
Oct 15, 2024 2:50 PM UTC

Hello @Dilip_Kumar 

the Peripheral Increment Mode should be set to DMA_PINC_DISABLE to keep the peripheral address constant. Additionally, you need to ensure that the data alignment settings match the requirements of the CRC peripheral.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om