Skip to main content
RAnan.3
Associate III
May 17, 2023 2:22 PM UTC
Question

C270 Camera integrating with STM

I use STM32L496RE controller to integrate C270 logitech camera using USB protocol. I got a sample link from the community https://github.com/iliasam/STM32_HOST_UVC_Camera.

The controller board I'm using acts as a USB host.

Since there were no defined classes for Video in ST's cube IDE, The code in the above link had a separate video class file written keeping ST's audio class file as basis.

Once the camera is connected I'm getting a interrupt from USB_OTG. I'm not able to move further after this.

Is there any other way to integrate logitech's C270 camera with ST?

Or Has anyone verified the above code on their project?

This topic has been closed for replies.