Skip to main content
T B
Associate III
Apr 14, 2025 6:36 AM UTC
Solved

Build doxygen

Hi,

when building the Doxygen documentation locally, numerous warnings appear. Especially, errors like this:

stm32g4xx_hal_driver/Inc/stm32g4xx_ll_lptim.h:605: warning: Found unknown command '@rmtoll'
stm32g4xx_hal_driver/Inc/stm32g4xx_ll_lptim.h:601: warning: found documented return type for LL_LPTIM_ConfigOutput that does not return anything
stm32g4xx_hal_driver/Inc/stm32g4xx_hal.h:431: warning: unable to resolve reference to 'SYSCFG_FASTMODEPLUS_PB8' for \ref command

 

Is there a Doxygen configuration for HAL?

What needs to be changed/added in the Doxygen default settings?

 

Thanks

Thomas

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Apr 14, 2025 7:11 AM UTC

Do you have a configuration file for the doxygen project? "rmtoll" is a custom macro, likely it means a connector between Reference Manuals (RM) and functions in the Low level drivers (LL). The LL layer has longer, more human friendly names. 

These custom macros can invoke custom actions, like look-ups in external databases and so on.

 

1 reply

Pavel A.
Pavel A.Best answer
Apr 14, 2025 7:11 AM UTC

Do you have a configuration file for the doxygen project? "rmtoll" is a custom macro, likely it means a connector between Reference Manuals (RM) and functions in the Low level drivers (LL). The LL layer has longer, more human friendly names. 

These custom macros can invoke custom actions, like look-ups in external databases and so on.