Skip to main content
MArgi
Associate II
Mar 14, 2019 10:21 PM UTC
Question

BUGs in STM32F0xx_StdPeriph_Lib_V1.5.0

I have been implementing firmware for STM32F042 and used the Std Peripheral library (v.1.5.0). I found the following bug(s):

Bug: DMA1_Channel4_5_IRQn() was never called

In file Libraries/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.h

Line 5558:

#define DMA1_Channel4_5_IRQn DMA1_Channel4_5_6_7_IRQn
  • DMA1_Channel4_5_6_7_IRQn is not defined for STM32F042
  • This line redefines (thus overwrite) an already correctly defined DMA1_Channel4_5_IRQn (line 344).

Line 5569:

 #define DMA1_Channel4_5_IRQHandler DMA1_Channel4_5_6_7_IRQHandler
  • DMA1_Channel4_5_6_7_IRQHandler is NOT listed in STM32F042x6.vec.
  • DMA1_Channel4_5_IRQHandler is actually the one in the vector table.

Possible fix: remove lines 5558 and 5569.

Minor issue: unused CANx generates warning

In file: Libraries/STM32F0xx_StdPeriph_Driver/src/stm32f0xx_can.c

Add following code to line 157:

 /* Unused CANx */

 (void)(CANx);

Resetting register in a confusing way

In file: Libraries/STM32F0xx_StdPeriph_Driver/src/stm32f0xx_can.c

Line 585: CANx->sTxMailBox[transmit_mailbox].TIR &= TMIDxR_TXRQ; 

Why don't simply assigning "TIR=0x00"? It's a bit confusing the usage of TMIDxR_TXRQ (=0x01) in this line. Of course, at that point TXRQ bit is set to 0, thus the result is TIR=0x00.

Marco

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Mar 14, 2019 10:29 PM UTC

Ok, and was that because it wasn't in the vector table, or that nothing enabled triggered it?

You're going to have to provide a worked example if you want people to review or fix things.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MArgi
MArgiAuthor
Associate II
Mar 14, 2019 11:05 PM UTC

I had accidentally posted the post while still editing it.

MArgi
MArgiAuthor
Associate II
Mar 19, 2019 2:39 AM UTC

Hi @Community member​ ,

Do you reckon my description is not enough? Should I add code?