Skip to main content
JLata
Visitor II
August 11, 2020
Question

BUG: v1.8.0 stm32h7xx_hal_spi in IRQHandler

There is a bug in the IRQHandler function that causes the callbacks associated not being correctly called.

 hspi->State = HAL_SPI_STATE_READY; 
 if (hspi->ErrorCode != HAL_SPI_ERROR_NONE)
 {
#if (USE_HAL_SPI_REGISTER_CALLBACKS == 1UL)
 hspi->ErrorCallback(hspi);
#else
 HAL_SPI_ErrorCallback(hspi);
#endif /* USE_HAL_SPI_REGISTER_CALLBACKS */
 return;
 }
 }
 
#if (USE_HAL_SPI_REGISTER_CALLBACKS == 1UL)
 /* Call appropriate user callback */
 if (State == HAL_SPI_STATE_BUSY_TX_RX)
 {
 hspi->TxRxCpltCallback(hspi);
 }
 else if (State == HAL_SPI_STATE_BUSY_RX)
 {
 hspi->RxCpltCallback(hspi);
 }
 else if (State == HAL_SPI_STATE_BUSY_TX)
 {
 hspi->TxCpltCallback(hspi);
 }
#else
 /* Call appropriate user callback */
 if (State == HAL_SPI_STATE_BUSY_TX_RX)
 {
 HAL_SPI_TxRxCpltCallback(hspi);
 }
 else if (State == HAL_SPI_STATE_BUSY_RX)
 {
 HAL_SPI_RxCpltCallback(hspi);
 }
 else if (State == HAL_SPI_STATE_BUSY_TX)
 {
 HAL_SPI_TxCpltCallback(hspi);
 }
	else
 {
 /* end of the appropriate call */
 }

When entering the IRQHandler, the "State" Variable is always "HAL_SPI_STATE_READY" therefore the callback functions are not called.

This topic has been closed for replies.