Skip to main content
samuel23
Associate III
Sep 16, 2025 12:40 PM UTC
Question

Bug suspected in .h with repercussions on HAL for STM32G4 (RNG macros)

Hi,

I discovered today with some of my students this potential bug in the stm32g431xx.h file:

 

#define RNG_CR_CED_Pos (5U)
#define RNG_CR_CED_Msk (0x1UL << RNG_CR_IE_Pos) /*!< 0x00000020 */
#define RNG_CR_CED RNG_CR_IE_Msk

As RNG_CR_IE_Pos is equal to 3... This mask is not correct.

It is quite strange: the comment is true... according to the Reference manuel 0440.

I suggest this correction:

 

#define RNG_CR_CED_Pos (5U)
#define RNG_CR_CED_Msk (0x1UL << RNG_CR_CED_Pos) /*!< 0x00000020 */
#define RNG_CR_CED RNG_CR_CED_Msk

 

 

(I checked the last version of this file using this official github : https://github.com/STMicroelectronics/cmsis-device-g4/blob/7c39c32593b03764aaa57531588b8bf7cdd443a5/Include/stm32g431xx.h )

 

In the HAL, the assert can't detect the fail... "checking itself" : 

assert_param(IS_RNG_CED(hrng->Init.ClockErrorDetection));

And this line used this CED... faking:

MODIFY_REG(hrng->Instance->CR, RNG_CR_CED, hrng->Init.ClockErrorDetection);

've fun...

Thx,

Samuel.

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
Sep 16, 2025 2:48 PM UTC

Hello @samuel23 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 217616 (This is an internal tracking number and is not accessible or usable by customers).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om