Question
bug on STM32_USB_Device_Library
Posted on December 08, 2015 at 10:20
Hi,
I found another bug on USB library for the STM32F3XX (STM32_USB_Device_Library in STM32Cube_FW_F3_V1.3.0). STM32Cube_FW_F3_V1.3.0\Middlewares\ST\STM32_USB_Device_Library\Core\Src\usbd_core.c In the usbd_core.c file, the function �USBD_LL_SetupStage� should check the bits [D6:D5] of bmResquest to identify the type request. The function doesn�t work for non standard request type. See USB2.0 specification chapter 9.3 table 9.2. So when I send to the device request with bmResquest =0xA2 (Dir=In, Type=Class, Recipient=Endpoint) used in USBTMC stack (USBTMC_InitiateAbortBulkOut), this request is badly parsed! Here is the right code for this function: /** * @brief USBD_SetupStage * Handle the setup stage * @param pdev: device instance * @retval status */ USBD_StatusTypeDef USBD_LL_SetupStage(USBD_HandleTypeDef *pdev, uint8_t *psetup) { USBD_ParseSetupRequest(&pdev->request, psetup); pdev->ep0_state = USBD_EP0_SETUP; pdev->ep0_data_len = pdev->request.wLength; /* bug should check if bmRequest is standard request type ! */ /* @see table 9.2 chap 9 of USB Spec ! */ uint8_t type = pdev->request.bmRequest & USB_REQ_TYPE_MASK; switch (type) { case USB_REQ_TYPE_STANDARD: switch (pdev->request.bmRequest & 0x1F) { case USB_REQ_RECIPIENT_DEVICE: USBD_StdDevReq(pdev, &pdev->request); break; case USB_REQ_RECIPIENT_INTERFACE: USBD_StdItfReq(pdev, &pdev->request); break; case USB_REQ_RECIPIENT_ENDPOINT: USBD_StdEPReq(pdev, &pdev->request); break; default: USBD_LL_StallEP(pdev, pdev->request.bmRequest & 0x80); break; } break; case USB_REQ_TYPE_CLASS: case USB_REQ_TYPE_VENDOR: /* added missing callback ! */ if (pdev->dev_state == USBD_STATE_CONFIGURED) { if (pdev->pClass->Setup != NULL) pdev->pClass->Setup(pdev, &pdev->request); } else { USBD_CtlError(pdev, &pdev->request); } break; } return USBD_OK; }This bug is also on all firmware.
#setupstage #bug #usb #stm32cube