Skip to main content
Associate III
Dec 5, 2024 5:49 PM UTC
Solved

Bug in stm32h7rsxx_hal_cortex.c -- MPU regions are never enabled

The net effect of this bug is that the reference code (including the Templates for LRUN and XIP) never actually enable the Memory Protection Unit regions.

See: stm32h7rsxx_hal_cortex.c Line 532 

I believe the second "Disable the Region" should have been an "Enable the Region", and called SET_BIT(MPU->RASR, MPU_RASR_ENABLE_Msk). 

Without this, the result after a call to HAL_MPU_ConfigRegion is a disabled region, requiring a second call to HAL_MPU_EnableRegion(). Note that there are no calls to this function in the H7RS reference code or templates. As a result, these regions are never enabled.

I discovered this issue when a region I marked as non-cachable was being cached despite the region specifically declaring it as NOT_CACHABLE.

 

 

 

This topic has been closed for replies.
FA1234Best answer
Associate III
Dec 5, 2024 5:57 PM UTC

Please disregard. I missed that the bit is overridden in the RASR set below. The dual CLEAR_BIT is probably not necessary, but seemingly harmless.

Now to figure out why my noncacheable region is still being cached...

 

1 reply

FA1234AuthorBest answer
Associate III
Dec 5, 2024 5:57 PM UTC

Please disregard. I missed that the bit is overridden in the RASR set below. The dual CLEAR_BIT is probably not necessary, but seemingly harmless.

Now to figure out why my noncacheable region is still being cached...