Skip to main content
fal.sch
Associate II
August 17, 2020
Question

Bug in stm32f3xx_hal_i2c.c

CubeIDE version 1.4.1

STM32Cube FW_F3 V1.11.0

I had the problem, that my I2C communication (alternating rx/tx on slave) works on the first rx/tx cycle but fails on the second tx.

The transmission skips the first byte and thus sending n-1 bytes. I found out that, after calling I2C_ITSlaveCplt() on line 4744, the execution of the function continues and decrements the XferCount on line 4802.

I fixed the driver as follows (original line 4740-4745):

/* Check if STOPF is set */
 if ((I2C_CHECK_FLAG(tmpITFlags, I2C_FLAG_STOPF) != RESET) && (I2C_CHECK_IT_SOURCE(ITSources, I2C_IT_STOPI) != RESET))
 {
 /* Call I2C Slave complete process */
 I2C_ITSlaveCplt(hi2c, tmpITFlags);
 }
/* Check if STOPF is set */
 if ((I2C_CHECK_FLAG(tmpITFlags, I2C_FLAG_STOPF) != RESET) && (I2C_CHECK_IT_SOURCE(ITSources, I2C_IT_STOPI) != RESET))
 {
 /* Call I2C Slave complete process */
 I2C_ITSlaveCplt(hi2c, tmpITFlags);
 
 // BEGIN BUG FIX
 __HAL_UNLOCK(hi2c);
 
 return HAL_OK;
 // END BUG FIX
 }

This topic has been closed for replies.

2 replies

fal.sch
fal.schAuthor
Associate II
August 17, 2020

Alternatively the following if-statement could be changed to an else-if-statement which is similar to the previous working driver version.

Amel NASRI
ST Technical Moderator
August 17, 2020

Hi @fal.sch​ ,

This issue is reported to our development team for farther check and analysis in order to apply the adequate solution.

Thanks for highlighting it.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.