Skip to main content
DOsbo
Associate III
Jul 3, 2019 3:56 AM UTC
Solved

Bug: HAL_DeInit() causes the STM32H7 microprocessor to reset.

Hi All,

Calling HAL_DeInit() causes the STM32H7 micro to reset when it executes __HAL_RCC_AHB3_FORCE_RESET();

#define __HAL_RCC_AHB3_FORCE_RESET() (RCC->AHB3RSTR=0xFFFFFFFFU)
 
HAL_StatusTypeDef HAL_DeInit(void)
{
 /* Reset of all peripherals */
 __HAL_RCC_AHB3_FORCE_RESET(); // <-- Causes CPU reset
 __HAL_RCC_AHB3_RELEASE_RESET();
.
.
.
}

I assume it is because it is writing 1's to reserved bits. Replacing the macro with the following fixes the issue:

#define __HAL_RCC_AHB3_FORCE_RESET() RCC->AHB3RSTR |= (RCC_AHB3RSTR_MDMARST \
| RCC_AHB3RSTR_DMA2DRST \
| RCC_AHB3RSTR_JPGDECRST \
| RCC_AHB3RSTR_FMCRST \
| RCC_AHB3RSTR_QSPIRST \
| RCC_AHB3RSTR_SDMMC1RST)

I hope this gets fixed in the next HAL release. It caused me a lot of headaches :)

Cheers,

David

This topic has been closed for replies.
lutztonineubert
lutztonineubertBest answer
Associate II
Jul 14, 2021 7:29 AM UTC

Sorry. As i see, it is fixed.

3 replies

ST Technical Moderator
Jul 3, 2019 9:19 AM UTC

Hello @DOsbo​ ,

We raised this issue internally for check and we will come back to you soon with update.

Thanks for your contribution.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Dec 26, 2019 12:39 PM UTC

Hello @DOsbo​ ,

Thanks for your proposal.

This issue will be fixed in the coming release.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
lutztonineubert
lutztonineubertBest answer
Associate II
Jul 14, 2021 7:29 AM UTC

Sorry. As i see, it is fixed.