Skip to main content
AWood.1
Associate
August 16, 2020
Question

Bug: cmsis_os.c The implementation of osMessagePut() does not agree with description

  • August 16, 2020
  • 1 reply
  • 631 views

The comments for osMessagePut() match osMessageGet() and note that

* @param millisec timeout value or 0 in case of no time-out.

However

osMessagePut() does not return immediately when millisec ==0. The code that is in osMessageGet() to handle this case is missing from osMessagePut()

Suggest replacing:

 ticks = millisec / portTICK_PERIOD_MS;

 if (ticks == 0) {

  ticks = 1;

 }

with same code as the Get():

ticks = 0;

 if (millisec == osWaitForever) {

   ticks = portMAX_DELAY;

 }

 else if (millisec != 0) {

  ticks = millisec / portTICK_PERIOD_MS;

  if (ticks == 0) {

   ticks = 1;

  }

 }

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
August 17, 2020

Hi @AWood.1​ ,

Thanks for sharing your proposal, I submitted your request to our development team for farther checks.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.