Skip to main content
Associate
Sep 25, 2024 5:41 AM UTC
Question

Brightness control on ST7789v TFT display using a STM board

I have a TFT display which outputs 320 X 240 pixels and I want to control the display brightness from the command itself which I found in the datasheet of the TFT display controller IC, so with the reference from the datasheet I have to trigger the WRDISBV in 51h and WRCTRLD 53h registers and in the 51h register I can vary the brightness from 0x00 to 0xff by passing any values in between, however after passing the command nothing is happening, I don't see any change in the brightness of the display.

How can I make this work using the command itself and not use any hardware to control the brightness?
Suggestions and ideas are welcome!

The link for the datasheet: https://www.rhydolabz.com/documents/33/ST7789.pdf

This topic has been closed for replies.

1 reply

MOBEJ
ST Employee
Sep 30, 2024 1:39 PM UTC

Hello @Akshay_ ,

To provide you an example with TFT Display , Please can you specify which STM32board are you using ?

Thank you 

BeST regards 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.