Skip to main content
Associate
Feb 1, 2026 10:45 AM UTC
Solved

Bootloader + XIP Application in External Flash on STM32U5G9J-DK2

Hello everyone,

I’m working with the STM32U5G9J-DK2 and trying to implement a Bootloader + XIP (Execute-In-Place) application architecture using the external flash.

Target setup:

  • A minimal bootloader running from internal flash

  • The main application linked to and executing from external flash (memory-mapped at 0x90000000)

The main motivation is to free internal flash and validate this approach for a future MCU with very limited internal flash.


What I’m specifically looking for help with

  1. Proper CubeMX / .ioc configuration for the bootloader

    • Which peripherals must be enabled (RCC, PWR, ICACHE, OSPI, etc.)

    • Which peripherals should not be enabled to avoid conflicts with the XIP app

    • Any STM32U5-specific gotchas when initializing OSPI for XIP

  2. Proper configuration of the application project

    • Recommended changes to the application .ioc

    • What initialization should be removed from the app (HAL_Init, clock, OSPI, FLASH, etc.)

  3. Reference samples

    • STM32Cube examples that demonstrate a full bootloader + XIP app flow on STM32U5

    • Any internal / unofficial sample projects that ST recommends adapting

I’m mainly looking for end-to-end guidance on how ST recommends structuring and configuring both the bootloader and the application for this use case.

Any pointers, samples, or best-practice recommendations would be greatly appreciated.

Thanks in advance,
AJ

Saket_OmBest answer
ST Technical Moderator
Feb 3, 2026 9:34 AM UTC

Hello @ArunJohn 

Unfortunately, there is no example XIP on STM32CubeU5. But you can get inspired from the example on STM32CubeF7.

STM32CubeF7/Projects/STM32746G-Discovery/Examples/QSPI/QSPI_ExecuteInPlace at master · STMicroelectronics/STM32CubeF7

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

6 replies

Associate III
Feb 1, 2026 9:21 PM UTC

Hello,

I did exactly now on this devboard RTC with additional functions like pictures slideshow and so on.

U5_RTC.jpeg

Maybe will be helpful the code of RTC project.

https://github.com/wegi1/STM32U5G9J-DK2-RTC 

 

What is the most significancy in support at this board and many other Discovery kit, that is the Examples pack shared in CubeMX. How I try to programming this boards it is not like you perfection setup peripherial one by one, just I use and look at the examples and copy BSP libraries. For example when I "wake up" external flash, I used BSP files and additionally in CubeMX set HSPI as enable without any settings made. All of this doing for me 1 line invoking BSP function:

status = BSP_HSPI_NOR_Init(0, &Hspi_NOR_Init);

And thats it. Whole function which read RAW data of picture into the frame buffer looks:

 

void readPicFromFlash(uint32_t pic_nr) {
	 /* HSPI info structure */
	 int32_t status;

	 uint8_t* pFBaddr;
	 uint32_t flash_offs;


	 status = BSP_HSPI_NOR_DeInit(0);

	#define FRAME_ADDRESS ((uint32_t)0x200C0000)

	 Hspi_NOR_Init.InterfaceMode = BSP_HSPI_NOR_SPI_MODE;
// Hspi_NOR_Init.InterfaceMode = BSP_HSPI_NOR_OPI_MODE; // if you want OPI
	 Hspi_NOR_Init.TransferRate = BSP_HSPI_NOR_STR_TRANSFER;


	 status = BSP_HSPI_NOR_Init(0, &Hspi_NOR_Init);

	 if (status != BSP_ERROR_NONE)
	 {
	 Error_Handler();
	 }
	 else
	 {
	 	pFBaddr = (uint8_t *) FRAME_ADDRESS;
	 	for(uint32_t i = 0; i < (800*480*2) ; i++) {
	 		pFBaddr[i] = 0;
	 	}
	 	flash_offs = 800*960*pic_nr;


	 		/* Read data from the HSPI NOR memory */
	 		if(BSP_HSPI_NOR_Read(0, pFBaddr, flash_offs, 800*960) != BSP_ERROR_NONE)
	 		{
	 			Error_Handler();
	 		}
	 }
	 status = BSP_HSPI_NOR_DeInit(0);
}

 

I'm not sure in this kit external flash can be mapped at 0x90000000  bcos external loader working at 0xA0000000:

U5HSPI.jpeg

The most important help I find in BSP example application in example pack.

This same way I did XIP and bootloader when I struggled with STM32H750B-DK - the example of bootloader is in the example pack, and rest is only change linker script file which have flash address changed. MEMBootloader take about 8KB and its doesnt matter when internal flash exists 128KB.

Most important in MEMbootloader is running external flash in memory mapped mode, what it doing without any problem bcos it exists in Bootloader example.

 

 

 

Other way is the "N" disco STM32N6570-DK 

 

 

N9_pic1.jpg

N9_pic2.jpg

 

where internal flash absolutly doesn't exists. It have only PROM which was programmed from factory with all possible bootloaders where you need running own program as first or second stage bootloader or application loaded by bootloader.

 

So maybe my programs are not perfect and literally used peripherials, but it is the fastest way to acheve communication with this hardware via BSP libraries. I'm not sure it is for you most desired style of code but it is :)

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Saket_OmBest answer
ST Technical Moderator
Feb 3, 2026 9:34 AM UTC

Hello @ArunJohn 

Unfortunately, there is no example XIP on STM32CubeU5. But you can get inspired from the example on STM32CubeF7.

STM32CubeF7/Projects/STM32746G-Discovery/Examples/QSPI/QSPI_ExecuteInPlace at master · STMicroelectronics/STM32CubeF7

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate III
Feb 3, 2026 10:03 AM UTC

1. If you need for cube ioc file properly initial values of enabled peripherials you can get it from initializations BSP procedures.

2. Also as mention before Saket_Om you can check and analyse examples of MemBootloader and XIP from STM32H750-DK which learned me how to do it.

NAmam.2
Associate III
Oct 14, 2026 4:04 PM UTC

Hello,

I am working on a similar requirement involving XIP (Execute-In-Place) from external QSPI flash on the STM32U5G9 and am encountering an issue executing the application from external flash.

I have developed a working external flash loader for my QSPI memory and successfully programmed a simple GPIO toggle application into external flash.

In the bootloader, I initialize the QSPI interface, configure the flash in memory-mapped mode, and then jump to the application located at 0xA0000000.

Using the debugger, I can confirm that execution reaches the application's Reset_Handler at 0xA00002B4. However, when executing the very first assembly instruction, the processor enters HardFault_Handler at 0xA0000458.

The fault status registers indicate:

  • CFSR = 0x00000001 (Instruction Access Violation)

  • HFSR = 0x40000000 (Forced HardFault)

  • MPU is disabled

  • VTOR = 0xA0000000

I have also verified that the application vector table contains valid stack-pointer and reset-handler addresses, and that the external flash contents can be read correctly through the debugger.

I am unable to determine why XIP execution is failing despite the QSPI memory-mapped interface appearing to work correctly.

Has anyone encountered a similar issue or have any suggestions on what I should check?

I would be happy to share my bootloader and application code for further review if needed.

Thank you in advance for your help.
Naga.

Visitor
Oct 20, 2026 8:23 AM UTC

@sportzfy

1. If you need for cube ioc file properly initial values of enabled peripherials you can get it from initializations BSP procedures.

2. Also as mention before Saket_Om you can check and analyse examples of MemBootloader and XIP from STM32H750-DK which learned me how to do it.

NAmam.2
Associate III
Oct 20, 2026 1:28 PM UTC

Thank you for the response, The problem is solved and XIP functioning properly after enabling the MPU.